STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SysTick not preempting other interrupts

Hello,I've got a very basic setup for an STM32G431KB/STM32G441KB where I use default interrupt priorities (verified all 0 in SBC and NVIC) for each exception in the vector table. I would therefore expect that a SysTick exception (-1) would preempt an...

danderle by Associate II
  • 3307 Views
  • 5 replies
  • 0 kudos

Resolved! How to choose an external crystal for STM?

The MCU of STM selects the external crystal, whether to choose a high frequency or a low one, what are the instructions?For example, for stm32L486, the datasheet gives the maximum main frequency as 80MHz, so 4Mhz, 8Mhz, 16Mhz, 20Mhz, 40Mhz can be rea...

SNorm.1 by Associate III
  • 7088 Views
  • 5 replies
  • 0 kudos

STM32F103VE <-> STM32F302CB I2C communication problem

Hello, teachers. I'm an introductory to stm32.I am posting like this because there is a situation where communication is not possible while communicating i2c between stm32.This is the current structure.STM32F103VE Use 1 Master, STM32F302CB Use 5 Slav...

JChoi.5 by Associate
  • 1589 Views
  • 2 replies
  • 0 kudos

Resolved! Please someone help me in finding the datasheet for STM32F072RB in order to look into the "Alternate function mapping" of the GPIO pins.

I am using STM32F072RB Nucleo board and in the technical reference manual it is mentioned that "Please refer to the “Alternate function mapping�? table in the device datasheet for the detailed mapping of the alternate function I/O pins.". But I am no...

HD.1 by Associate
  • 1436 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030C8 GPIO Max Source Current is limited to <5mA

Device Used : STM32F030C8, 48pin LQFP48I am driving MOC3043 Opto-Isolated Triac Driver so I need atleast 5 mA current sourced from the GPIO outputGPIO used with the MOC3043 is PA15 max current observed is 4.86mAOnly a single GPIO is configured at a t...

NFern.1 by Associate III
  • 5000 Views
  • 4 replies
  • 0 kudos

Adc using DMA for sine wave

Hi,​ Iam using DMA technique to digitise a sine wave using nucleo-H743ZI2, where Adc clock frequency is 36.5MHZ . Iam taking single data at a time and sending out using usart with a baud rate of 250000, the issue I am facing is when I increase th...

GHARI.1 by Associate II
  • 5813 Views
  • 12 replies
  • 0 kudos

How to debug both cores of the STM32H745 simultaneously?

Hello!i am working with the stm32h745 nucleo 144 board.i want to be able to debug both cores simultaneously using the onboard STLINK debugger, with no luck so far.followed the instructions from this ST document: https://www.st.com/resource/en/applica...

yuri CH by Senior
  • 1516 Views
  • 2 replies
  • 0 kudos

How should I build an effective peripheral "driver" ?

I've spent a fair amount of time getting small bits of code working so I can build them up into a larger working application. The code below works but I'm struggling with a way to move the parts related to GPS and the UART into separate files or clas...

magene by Senior II
  • 1190 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.