STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FT5426 Not respond MCU

I am working with stm32f7-custom board using 8inch touch screen(microe3902) & FT5426 capacitive touch controller FT5426 not respond properly

Resolved! Problem connecting SPI to

I am new to STM32. I am porting my code from ATMega128 to STM32 for faster thru put . I have to connect W5500 to STM32F103 on SPI2. To test my understanding of SPI on STM32 after compiling , a small test code in while loop.  SPI_Write(S0_CR,CR_CLOSE)...

CK.3 by Associate III
  • 3084 Views
  • 7 replies
  • 0 kudos

ScrollWheel giving build error.

Hello,In my project, when ever I use a scroll wheel widget, visual studio is giving build errors in base files. Can anyone please state a possible reason?

0693W00000FBaS3QAL.png
Revanth by Associate III
  • 809 Views
  • 0 replies
  • 0 kudos

DFSD with two PDM mics using a single input

Hi,I followed the example for DFSDM found in DM00380469_ENV1.pdf and setup the channels as specified (channel 0/1 -> input from ch1 and internal clock). Cube MX also creates 2 pins , CLK and DATAIN1.STM32F413 MCUIt seems that I cant get any data comi...

NKara.3 by Associate II
  • 2321 Views
  • 3 replies
  • 0 kudos

Cannot use CAN on alternate pins

Part is STM32L4Q5CGIf configured to use PA11 and PA12 on AF 9 works as described in programming reference. When changing pins used to PB8 and PB9 CAN cannot be used and never leaves reset. On my custom board I have PA11 and PA12 in use by USB so I ca...

DPlum by Associate II
  • 2679 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.