STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 CAN2 normal mode not working

Hello,I have problem in CAN2 STM32F4, that in mode Loopback working good, but when i change it to mode Normal not working (not transmission )Please do you have a solution for working in the mode Normal ?

MBRAH.1 by Associate
  • 1244 Views
  • 1 replies
  • 0 kudos

STM32H7 - Sending CMD5 to eMMC card

Hi,I'm working with an STM32H7 connected though SDMM1 (1bit bus width) with an eMMC, I need to put the eMMC into sleep mode so we can reduce the power consumption when it is not being used.According to the information I've been able to find we need t...

CDiaz.2 by Associate II
  • 1736 Views
  • 1 replies
  • 0 kudos

Signal Integrity Simulation with IBIS model of STM32H7B3IIK6

Hello.I have got the IBIS model of STM32H7B3IIK6 from ST website, but there is no document to explain how to use this IBIS model. As there is so many sub-models included, I don't know what model I should selected for the FMC data pin, e.g. io8_ft_fs_...

WLiao.1 by Associate II
  • 1355 Views
  • 1 replies
  • 0 kudos

Raw RNG samples STM32F7: has anyone already tried it?

Hi,I am actually trying to collect raw samples from TRGN module of a STM32F7.To be more clear, raw sample means unprocessed data coming directly from the source. It is possible using a special IO configuration setup and external equipment in order to...

MLave.2 by Associate II
  • 2019 Views
  • 4 replies
  • 0 kudos

I2C flag RXNE automatically clear before read register

I initiate reception from the microcircuit for stm32h723. However, the code hangs while waiting for the RXNE flag. In the debug, step by step, you can see that the flag is set after START, but is immediately reset to zero in the next step, before che...

NBoga by Associate
  • 1137 Views
  • 1 replies
  • 0 kudos

STM32L4: COMP1 and COMP2 as TIM1 BREAK2 input sources.

Hi,I am using STM32L476 MCU. I have COMP1 and COMP2 configured in window mode. That's working fine. I would like to have COMP1 and COMP2 as break input sources for TIM1 BRKIN2. Test #1: if I set COMP1 as break input source, that works:LL_TIM_EnableBr...

MGard.2 by Associate II
  • 1577 Views
  • 1 replies
  • 0 kudos

UART Overrun error

Hello,I transfer data by uart interrupt(Uart_RX_IT_Start()).Now UART overrun error is occurred continuously.Should I have checked any point?I want to use the uart interrupt, not DMA.Thanks.

Kim.Andy by Associate III
  • 2012 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.