STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L011 how to reach 1uA in standby mode?

Hello. I have been getting familiar with the STM32L011F4P6 chip. I am using a 20-pin chip soldered onto a board as my test device. I am using a Nucleo-f429zi as the programming/debug device. I have made the necessary changes and am using the SWD head...

AW.3 by Associate II
  • 3867 Views
  • 6 replies
  • 0 kudos

MCU with IO bandwidth of 150Mhz or more

Hi All,He have an application that requires fast IO's switching. More specifically, we have a 16bit 200Msps parallel DAC and we are targeting to load a waveform from either flash memory or external memory and output the bits for the DAC. Using an FPG...

VVarg.1 by Associate II
  • 2656 Views
  • 4 replies
  • 0 kudos

Serial routine fails for some reason

STM32F429ZIT6 - NucleoI am doing some tests with this board, it reads Encoder input in x4 mode, generates TRGO to ITR1 slave TIM1 in One pulse mode when it reaches TIM2->CCR3 value and updates Encoder counts and number of triggers every 15 seconds on...

DPatr.2 by Associate III
  • 1030 Views
  • 2 replies
  • 0 kudos

I'm following this tutorial: https://www.youtube.com/watch?v=WgsXMVZfoO8&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=7&ab_channel=STMicroelectronics And my boar cannot conect to mi phone.

The connection green led indicator doesn't twinkle, it is alway on and I can't see the nucleo in the ST BLE Sensor app. I suppose that the problem is with the CPU 2. I was debugging the code and it nevers reaches the function APPD_EnableCPU2( ); beca...

PGarg.1 by Associate II
  • 1646 Views
  • 2 replies
  • 0 kudos

"locked out" from Nucleo-L4P5, cannot erase or program

I have a Nucleo-L4P5ZG board and I cannot use it.Flash download in CubeIDE always fails because of an error erasing memory.I then hooked it up to STM32CubeProgrammer, but the problem persists.Independent whether I try to erase an individual sector or...

b.a. by Associate III
  • 988 Views
  • 2 replies
  • 0 kudos

STM32F7 CAN BUS Rx Interrupt not triggering

PREMISE: I have experience with other communication protocols but very little with CAN so I am not completely sure how to set the prescaler and other parameters.GOAL: I want to read a sensor (namely the airspeed sensor ASPD-DLVR) through the CAN BUS....

0693W00000GWoG2QAL.png 0693W00000GWoFnQAL.png 0693W00000GWoFiQAL.png
FUs.1 by Associate III
  • 1127 Views
  • 1 replies
  • 1 kudos

ADC interrupt never gets called

Hi, i'm struggling with this piece of code here:int main(void){ UART2_Tx_init(); ADC_interrupt_init();     while(1){   }   }   /***********ADC***********/   void ADC_interrupt_init(void){ RCC->AHB1ENR |= (1U<<0); //GPIOA clock enable GPIOA->MOD...

Nick- by Associate II
  • 1678 Views
  • 2 replies
  • 0 kudos

Resolved! Compare event of a general purpose timer and DMA request

I am using the nucleo L476rg and I am not sure to correctly understand the notation in the manual: I want a compare event of a timer to send the DMA request but in the DMA selection register is generally reported TIMx_CHx as request sender.Considerin...

Tommino by Senior
  • 1984 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.