STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error in RM0432 Rev 9 for MCOSEL[3:0]: Microcontroller clock output ? EDIT: Sorry, no error in the manual.

In the manual P 263:Bits 27:24 MCOSEL[3:0]: Microcontroller clock output Set and cleared by software. 0000: MCO output disabled, no clock on MCO 0001: SYSCLK system clock selected 0010: MSI clock selected. 0011: HSI16 clock selected. 0100: HSE clock ...

About starting and stopping a timer by an encoder timer

Incremental encoders are known to have problems for speed measurement at low speeds. For this, period measurement at low speeds is recommended.The following statement is taken from RM0440 page 1158. What I want to do here is to start another timer in...

0693W00000LxdfeQAB.png

Resolved! STM32F4 DMA FIFO + SPI_TX = FIFO error, but work

Good afternoon! I am trying to establish the transmission of data via SPI to the display with DMA. The transmission is working, the display is completely painted over, but the FIFO error flag is set in the DMA registers.MCU: STM32F401CEU6 alignas(32)...

DVahr.1 by Associate II
  • 3376 Views
  • 4 replies
  • 0 kudos

bxCan Filtering

I've been reading several forums posts about filtering, and other resources such as:https://community.st.com/s/question/0D50X00009XkfSlSAJ/can-filtershttps://blog.csdn.net/flydream0/article/details/52317532I get the gist of this.CAN_FilterIdHigh is t...

We are using STM32F103xB. We intend to replace STM32F103xB this with STM32F103xC, STM32F103xD & STM32F103xE. We found difference in memory map section in the "Aliased to Flash section", when comparing both MCUs. Will there be a need for Software change?.

We are using STM32F103xB. We intend to replace STM32F103xB this with STM32F103xC, STM32F103xD & STM32F103xE. We found difference in memory map section in the "Aliased to Flash section", when comparing both MCUs families. There is a section called re...

AKuma.43 by Associate
  • 1450 Views
  • 1 replies
  • 0 kudos

MDMA_STM32H7xx

HI. there are two TIM1 registers and you need to move its address 0x40010034 from one register to another register 0x40010038 exactly 64bit, that is, a double word. is it possible to do this with MDMA single? the documentation is very poor. I had to...

MTS by Associate II
  • 819 Views
  • 0 replies
  • 0 kudos

Reading a very slow PWM frequency

Hi,I need to read a PWM that a rotating wheel generates (16 pulses per revolution) and I want to use one of the STM32F429 timers to do it. The problem is that the period goes from 7.8ms to infinite (no pulses), so I don't know what will happen if the...

RMira.2 by Associate
  • 1053 Views
  • 1 replies
  • 0 kudos

synchronous communication problem

In one of our projects, we used stm32l031 microcontroller to make synchronous communication operating at 5Khz frequency. Total data length is 35 bits, 3 bits are the Id identification bit from the master device, the remaining 32 bits are data bits an...

HGüle.1 by Associate II
  • 2163 Views
  • 4 replies
  • 0 kudos

How to use peripherals in both core?

Hello,I am working on Nucleo-h745ziq board. I am enable the UASART3 ,the intialization in done in cortex m7 and I try to use in both core,but only core 7 USART3 is working in core m4 USART3 is not get worked ,the code is as followscore m7 code: HAL_U...

MDeva.1 by Associate II
  • 1206 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.