STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_RTC_GetTime return 1 instead of 13

Hello ST community! We're using STM32F401RDT6.We use the RTC to maintain scheduled events that occur in the time we set, but not with the RTC's Alarm mechanism, rather our custom-made mechanism based on the current epoch time which is being updated e...

RLand.2 by Associate II
  • 2481 Views
  • 2 replies
  • 0 kudos

How to read the current DMA buffer pointer correctly?

Hello, I'm using an stm32f429zit6's ADC in triple interleaved DMA mode. They're giving me 7.2 Msps currently.The ADC is continuously running in circular mode and filling a buffer with a size of 3000.So I wanted to find out the DMA buffer pointer when...

MMoha.3 by Associate III
  • 2945 Views
  • 3 replies
  • 0 kudos

Interfacing STM32 MCU to micro-LED (µLED) display.

Hi Community,I am working on Interfacing STM32 MCU to VGA LED display through SPI protocol.Display Power Requirement. 1) Core Supply Provided : 1.2V, 1000mA. (required 200mA)2) IO Supply : 2.5V, 1000mA. (required 200mA)3) Cathode Supply : -2V, 200mA....

Vins by Senior
  • 1479 Views
  • 2 replies
  • 0 kudos

About ADC_DMA_PROJECT(STM32H7)

Hello,I am working on the ADC_DMA_Transfer projectI have a question about MPU settings.The following code was executed when the MCU was initialized:Should I always run this code?//////static void MPU_Config(void){ MPU_Region_InitTypeDef MPU_InitStruc...

forst by Associate III
  • 2802 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.