STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Retriggering pulse

Hello dear friendsI use the stm32f4 series. I am looking for some code to retrigger a similar pulse. To be clear, I have some circuits for zero-cross detection. Now, for each input pulse before the next in[ut pulse, I want some output pulse that woul...

STM32, I2C HAL functions and RD5807M

Hi all,I'm having a very hard time with the use of HAL_I2C functions to communicate with a FM digital chip. This IC has two modes of communication: (1) a sequential mode used to send several bytes successively in the registers and (2) random mode to ...

dliky2 by Associate II
  • 2082 Views
  • 1 replies
  • 0 kudos

STM32G0 Flash program fast on non last erased page

Hello dear all,On STM32G0B0 I try to performe a Flash programming fast after erasing 2 pages on bank 2.1�?⃣ Erase code :uint32_t PageError; FLASH_EraseInitTypeDef tEraseInit; tEraseInit.TypeErase = FLASH_TYPEERASE_PAGES; tEraseInit.Banks = FLASH_BANK...

0693W00000NrCuTQAV.png 0693W00000NrCuYQAV.png 0693W00000NrCusQAF.png 0693W00000NrCvRQAV.png
MTE_MMO by Associate
  • 1873 Views
  • 0 replies
  • 0 kudos

ADC stays in LOCK with polling method

I have a project where i use the HAL library to poll the ADC.Controller STM32G473VC. Cube IDE 1.9.0.During the code i call ADC_24V_getADCvalue() at different places but never in interrupt routines .Even though after a few calls HAL_ADC_ConfigChannel ...

sde c.1 by Senior II
  • 779 Views
  • 0 replies
  • 0 kudos

Resolved! continuously read few register on SPI slave device, using DMA?

Master is a STM32H757, slave is a LSM6DSO ( accelero + gyro ).I have a SPI link inbetween.The "int2" pin on the LSM6 rise up when data are readable in registers.This pin is connected on EXTI2 on STM32.Register read is auto incremental on LSM6.I need ...

baptor by Associate III
  • 1957 Views
  • 1 replies
  • 1 kudos

Storing const value to ROM

Hello, is there a way to instruct the compiler to place a const value at a specific address in flash memory? On another toolchain I was able to useconst char array1[4] = {1,2,3,4} absolute 0x9D008000; // stored at flash address 0x9D008000If not, is...

MHast.1 by Associate II
  • 1652 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F7, ART vs ICACHE?

I'm starting with STM32F767 and cannot understand the thing about connection of the ITCM to ART. What is recommended: enable ART and flash access over TCM, or just enable ICACHE like in H7, and access code over AXIM?When flash is accessed via TCM, do...

Pavel A. by Super User
  • 1574 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.