STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why timer 8 has in TI1 the CCI4 label name?

Hi, I cannot understand why the TIM8 has in TI1 the label CC4I and the general purpose timer has at TI1 the label CC1I as you can see on the following pictures. And also I want to ask what is the different between TIM8 and TIM1 as advanced control ti...

0693W00000NrimHQAR.png 0693W00000NrimCQAR.png
NTosi by Associate III
  • 1802 Views
  • 3 replies
  • 1 kudos

STM32G0B0 - Timer with Interrupt issue

Code is very simple, not so many configs.Issue arises when I call HAL_TIM_Base_Start_IT(&htim3):/* Enable the TIM Update interrupt */ __HAL_TIM_ENABLE_IT(htim, TIM_IT_UPDATE);and code broke with no error on the Call Stack.I tried the same code on NU...

SMari.1 by Associate
  • 786 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB pairing error with mixed bonded/nonbonded devices

Hi,I am running a system with some STM32WB, one client and some server.Right now i am connecting, pairing and bonding the devices. If i start from a condition where i have all the server not bonded (aci_gap_get_bonded_devices return nothing) and I st...

LSpad.1 by Associate III
  • 4546 Views
  • 6 replies
  • 1 kudos

FDCAN classic in stm32h7 stop receiving data after some time

Hi, Am interfacing STM32H743 FDCAN classic with STM32F7 CAN. When I tried transmitting data from F7 to H7, within a minute H7 stop receiving data. I also tried debug the problem on F7 side and found that breakpoint hit on following condition inside t...

RJain.1 by Associate III
  • 981 Views
  • 0 replies
  • 0 kudos

Flash writing issue

Hi I'am using two different boards stm32f411 and stm32h723zg, so I am trying to write one byte data on flash which is 0xFF -> 0x70-> 0x10 -> 0x00 on same address in the sequence without erasing the flash, it’s working for stm32f411 but it doesn’t sup...

IK by Associate
  • 1005 Views
  • 1 replies
  • 0 kudos

What is 0.5 bits or 1.5 bits?

I understand that what is shown in the picture is wrong, I just do not know how else to describe it.0.5 bit is 50% duty cycle?And 1.5 bits is 150% duty cycle?If the percentage of filling changes by 150%, then the data transmission frequency must also...

0693W00000NrgMRQAZ.png
MMust.5 by Senior II
  • 4955 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.