What does the last letter U mean for this model “STM32H750XBH6�?
What does the last letter U mean for this model “STM32H750XBH6�?
Ask questions, find answers, and share insights on STM32 products and their technical features.
What does the last letter U mean for this model “STM32H750XBH6�?
I trying to debug my simple "Blink" code by pressing "STEP Over (F6)" but it freeze every time at SCB_ENABLEDCACHE ();But, if i press restart and "F8" (resume) everything working well! My stm is STM32H750VBT6.
Hi everyone, i see a warning when i write the code;--> HAL_UART_Receive(&huart3, &Rx_Byte[0], 1, 10);Rx_Byte is;--> char Rx_Byte[1];Why i see this warning can anyone help me?
Hello guys,I am using the stm32f446re discovery board, my aim is to measure the ram consumption of my application. The first approach is to use the static stack analyzer checking the memory details, the second approach is to fill the memory with a pa...
Hi everyone, Iam trying to integrate the wifi module(CC3100-Simple link)driver files with the stm32f1 microcontroller.1.After adding the required simplelink driver files with the STM32 code compiled and checked it but getting compile time errro...
hello,The option byte is configured with read and write protection, but I can program without erasing, why?FLASH_OBR = 0x03FFFFFAFLASH_WRPR = 0xFFFF0000
My company uses the STM32G0071CB chip. but I faced some issue.whenever I need to reboot main board, I have to reset the STM32G0071CB as wells.so I used the WWDG for resetting the chip.But sometimes, chip was not reset and CPU hang.(once a 400 times o...
Hi I need to place the math standard library in a specific memory section (otherwise, It won't be linked appropriately - luck of space)so I add to the ld file the following lines: .mylib : { . = ALIGN(4); *(.lib*); *(.libc) *(.libm) *(.libdsp); ...
Hello,I have tried implement UART Driver only with LL Library. I'm using Nucleo-H745ZIQ. Reception through DMA is not happening. Data is not getting copied to the buffer. MPU Also Configured. I'm attaching the code. Hope DMA Configuration for Rx is o...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.