STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Output voltage characteristics of STM32G070CB

Hello folks,I can't figure out the meaning of table 48 p.64 of STM32G070CB datasheet (see attached picture). In particular the FT_c pins. Page 63 it is written that all I/O can source up to +-6mA and +-15mA with relaxed VOL and VOH.Back to table 48, ...

0693W00000WJismQAD.png
Kraal by Lead
  • 2212 Views
  • 4 replies
  • 0 kudos

Resolved! Use RTC wake up in STM32F051 stop mode

Hello.​I am using the stm32f051 discover board.I want to use RTC's WAKE UP function when I wake up in stop mode, is there a way?​The STM32F051 MCU must be used.

THwna.1 by Associate
  • 3097 Views
  • 7 replies
  • 0 kudos

CANBUS nmea 2000 phrase protocol packet on STM32

I have STM32 microcontroller F4 I want to configure the GPS sensor for getting data, I used CANBUS cable and the protocol is nmea 2000, and communicate with HAL_CAN interrupt. my question is, how can I phrase the data from the sensor (on nmea 2000). ...

TBen .1 by Associate
  • 1588 Views
  • 0 replies
  • 0 kudos

I am using the microcontroller in the Nucleo L031K6 model. Our lecturer wants to control LEDs that change according to voltage using ADC and HAL library.

A potentiometer is connected to the breadboard, the middle leg of the potentiometer is connected to the adc pin and the other legs are connected to gnd and 5v.Led (Led Voltage <1V) - Led will be offLed (1V<Led Voltage <2V) - Led will blinkLed (2V < L...

0693W00000WJdF1QAL.png

Resolved! I2C not working with STM32F103C6 and STM32F103C8

we have been trying to get the I2C up on both the controller and no responses from anyone the cubeMx issue if I2C is really a problem..Kindly respond as we are trying to get I2C up ..requesting the experience forum experts to respond.Thanks Ravi

RShiv.1 by Senior
  • 58535 Views
  • 63 replies
  • 0 kudos

Why UART sometimes print twice the message?

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body *****************************************************************...

0693W00000WJgJGQA1.png
ATeli.1 by Associate III
  • 5684 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.