STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Memory Overlap with External QSPI

I have a QSPI Flash connected to the STM32H70 and it's all been terrific until I realised I can't address the FLASH's (a W95Qxx with 8M) full capacity with my current settings...How can I (or is it even possible to) change the memory address of the e...

STM32L5 lockup, Pulling nRST to GND does not reset

STM32L562I have the IWDG set up to fire 4 seconds if no HAL_IWDG_Refresh(&hiwdg) is executed.Very occasionally, a lockup condition occurs.But the STM32 does not reset.Moreover, grounding the nRST pin does not reset the STM32Scoping the nRST pin, i ca...

MLint.1 by Associate II
  • 6305 Views
  • 8 replies
  • 0 kudos

Resolved! STM32F303CBT6 TIM input interconection

Hello,The COMParator have option of connection him output to TIMer IC.But timer IC is after edge detection unit.How can I connect the output of COMPx to TIMx in input capture mod (internaly)?

AOrlo.2 by Associate II
  • 1976 Views
  • 2 replies
  • 0 kudos

How can I convert UART and I2C inputs to UART and CAN outputs?

Hi, I’m new to STM32.With STM32F730R8T6 MCU;I want to see the data using CAN protocol and UART protocol while sending data using UART protocol.At the same time, I want to see the data using CAN protocol and UART protocol while sending data using I2C ...

Macun by Associate II
  • 7257 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.