STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to setup DMA from timer to memory

I'm very new to the STM32 and am trying to set up TIM2 to trigger a dma input capture to memory. I have been pouring over examples and the STM32F302R8 ref manual but am not there yet.What is working is I am inputting 30Hz ref signal on both PA5 and ...

BTrem.1 by Senior II
  • 7365 Views
  • 6 replies
  • 0 kudos

Timer PWM settings

Hi,I am trying to use timer pwm outputs for Timer4, Timer2 and Timer1 bolcks. I am using initial functions below, but i can not see pwm signals from outputs. What is wrong with the codes below ? Any advises./**TIMER2 PWM SETUPS**/ RCC_APB2PeriphC...

er3481 by Senior
  • 1969 Views
  • 2 replies
  • 1 kudos

Input Capture Interrupt Problem

Greetings Everybody,I am using STM32F429I-DISC1 BOARD version MB1075 C-01. My main aim Generate square wave from 1HZ to 20KHZ - This is completed. I am using Timer5 to generate square wave as per my requirement. I have even checked it on oscillo sco...

A CCR3 issue on all timers

Hello everyone,I am starting to program with a stm32f103c8 and I have a problem when I want to update the compare output on channel 3. The output is either 0V or 3.3V depending on the polarity.The rest of the outputs work correctly.Here I leave the i...

kTC30 by Associate II
  • 2194 Views
  • 5 replies
  • 0 kudos

Jump To Application From

Hello,I am working on a custom bootloader for STM32F105 which it is possible to write a bin file into the flash via CAN bus(CAN2). My issue is that the part of bootloader to jump to application doesn't work. Here is the jump function code:#define MAI...

NASI by Senior
  • 12614 Views
  • 19 replies
  • 1 kudos

Resolved! SPI buffer TXDR was written as 0x00 .

I'm developing SPI driver for Nucleo-H753ZI so Nucleo-H753ZI will be SPI master. It'll be connected to DAC which is slave. As of now I'm using STM32HAL drivers to configure Nucleo-H753ZI as a Master. After configuration I've tried to transmit buffer ...

Problem with writing the DBANK option byte on STM32G474RE

Hello,I'm using the NUCLEO-G474RE development board and trying to set the DBANK option byte. I can do that using STM32CubeProgrammer without any issues, and everything works as it should.But when I try to do that in the firmware using the HAL functi...

DGrgic by Associate II
  • 1972 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.