STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Put function in RAM

Hi,how can I tell to the compiler that I want a function to be executed in RAM ?

DGo.1 by Associate II
  • 7834 Views
  • 9 replies
  • 1 kudos

Nucleo-U575ZI-Q running the ADC_SingleConversion_TriggerSW_IT shows wrong ADC results as soon I activate oversampling ?!

Init-Sequnece: hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.GainCompensation = 0; hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE...

Where is the STM32F103 start code?

Hi,As far as I understand, for the STM32F103, after a reset or power on without the use of the bootloader, the first task that happens is load SP with the content of address 0x00 (alias of 0x8000000) , followed by the load of the content of address 0...

carlossp by Associate II
  • 5324 Views
  • 5 replies
  • 0 kudos

Timer Input capture auto restart

Hi, I'm making a simple firmware to measure the frequency of some clocks, I'm using a timer IC + DMA, like this:HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, CH1_captures, 2);Then in the callback I do this:void HAL_TIM_IC_CaptureCallback(TIM_HandleType...

Timer triggered DMA doesn't work

I want to sample GPIO state twice per millisecond with DMA.I used TIM16 as basic counter - setting TIM16 CR1 register to 1, ARR to 32000 (half milisecond) and TIM16 DIER register to enable DMA on update (bit 8).Timer is checked to work fine. DMA doe...

WojtekP1 by Associate III
  • 2681 Views
  • 5 replies
  • 0 kudos

Resolved! Does STM32F767ZI support Battery charging detection (BCD)?

Hello team!I am newbie in STM32 world so probably i am missing something but please clarify this for me. I have found conficting informations:Datasheet "DS11532 Rev 7" at p. 47 says "Battery Charging Specification Revision 1.2 support"Reference Manua...

ŁJura.1 by Associate II
  • 1797 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.