STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clipped sine TCXO clock for STM32G031G8U6

The STM32G031G8U6 in a UFQFPN28 package does not have PF0 / PF1 pins for HSE OSC_IN / OSC_OUT.  It does however have OSC_IN on PC14.  This is intended for an external CMOS oscillator in bypass mode.I’m currently in the schematic design stage. My boar...

BK1 by Associate II
  • 787 Views
  • 6 replies
  • 0 kudos

3.3V stm32u5 and 1.8V PSRAM

Hi! I'm trying to design a project that will use an stm32u5, and I would like to add PSRAM to it. Most higher-capacity PSRAMs seem to want to run at 1.8V rather than 3.3V, from what I can tell.  The particular U5 I've tentatively selected (the U595),...

sb_st by Senior II
  • 378 Views
  • 5 replies
  • 3 kudos

STM32G4 UART Signal Handler Error

Hi there, I have firmware that uses UART1 and UART2 of the STM32G4 series. Both are intended to run on interrupts, but as soon as any signal is received by the MCU, an error occurs, causing HAL_UART_AbortCpltCallback to be called. Therafter, the inte...

Resolved! STM32U575CGU3 CAN Cycle Time Issue

I am using the STM32U575CGU3 MCU in my project, where I transmit data using two CAN frames on the bus. I have configured a CAN transmission cycle time of 250 ms in my software. However, on a few PCB assemblies, I am observing inconsistencies in the ...

Resolved! STM32H563RGT6 running at 125℃ environment

Hello ST,We are using STM32H563RGT6 and want to run at 125℃ environment.We see in the datasheet as below.it seems that for STM32H563RGT6 with suffix 6, if we are using LDO bypass mode (using external 1.2V power supply for MCU Vcore), MCU works at VOS...

lyan2_0-1778039564635.png
lyan.2 by Associate II
  • 247 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.