STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC is getting set off by 1hour in STM32U5. I am using Nucleo board and I am checking the RTC behavior in STOP3 mode of stm32u5.

#include "main.h" #include <stdio.h> #include <string.h> RTC_HandleTypeDef hrtc;   UART_HandleTypeDef huart1;   /* USER CODE BEGIN PV */ #define UartHandle &huart1 #define RtcHandle &hrtc static uint16_t YearStart = 2000;   char message[50]; uint8_t ...

STee.3 by Associate II
  • 2357 Views
  • 2 replies
  • 0 kudos

STM32F103C8 PWM with DMA

Hello,I'm using Timer_2 channel_1 PWM with DMA to generate the low polarity Pulse.I set the value of PSC = 72, ARR = 2000 and Fosc = 72 MHz.uint16_t TIM2_CCR1_Value[25] = {2100, 2100, 2100, 2100, 2100, 2100, 2100, 2100, 1200, 1500, 1500, 1500, 1500, ...

0693W00000aJ1xGQAS.jpg

SPI to read ADS7953 with STM32F072 not working.

HelloI am developing a board to measure many voltages for a student project. On that board are a ADS7953, a ISO7741 and a STM32F072. Now I am at the end of my resources. I can't read anything useful from the ads. Btw I am using an ADS7953 EVAL Board,...

LSant.6 by Associate II
  • 3236 Views
  • 1 replies
  • 0 kudos

STM32H7 HAL Read GPIOC13 with DMA into SRAM

Hello there, I am trying to read GPIO pins (on row C) with DMA into SRAM, using TIM1 as clockI am using STM32H750B-DKEssentialy, when TIM1 goes high DMA should read from GPIO to SRAM continuously (until its stopped by a user :))Here is what I tried s...

MKocj.1 by Associate II
  • 1874 Views
  • 3 replies
  • 0 kudos

ADC is weird too...

It is a quick learning project of LL driver programming on NUCLEO-L432KC. First I got a bug in MX configuration. It was fixed by ST:https://community.st.com/s/question/0D53W00002BCrfpSAD/the-simplest-and-most-basic-ll-driver-app-doesnt-workI then wen...

0693W00000aJRpFQAW.jpg 0693W00000aJS9cQAG.jpg
WQ by Associate III
  • 1514 Views
  • 1 replies
  • 0 kudos

Resolved! High current absorption issue in Low power sleep and stop mode

I'm trying to minimize the current consumption of an STM32G031K but I can't reach the ones calculated by the STM32CubeMX in any way. I tried with Low Power Sleep Mode, Stop Mode 0 and Stop mode 1. In Stop Mode 1, according to STM32CubeMX I should hav...

SPozz.1 by Associate III
  • 2760 Views
  • 2 replies
  • 0 kudos

How to calculate max encoder frequency

I'm using the encoder mode of the hw timer on a STM32G0 to count pulses of a quadrature encoder, and trying to figure out how fast the encoder can be run before we start to lose pulses. For reference the encoder is 10k CPR, and is on a wheel that can...

Konami by Senior II
  • 3748 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.