STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SRAM Memory write or erase getting a hardfault

Hi team, can anyone help me what is wrong im doing in the code, ihave used the SRAM(1/2/3) or part of SRAM which is SRAM1, the data is getting erased or written to the specified address but at the end its getting hard fault, can anyone help me to rec...

meghasb by Senior
  • 1540 Views
  • 2 replies
  • 0 kudos

HELLO! STM32L051R8T6 it has a problem with the initialization of the LSE / LSI clock?

After the analysis, we know that the processor in the system is powered by a battery voltage of 3.6 V and cyclically/after meeting certain conditions, it goes into Standby mode. It is woken up by the wakeup pin. After waking up, the processor correct...

锋赵.1 by Associate
  • 1606 Views
  • 1 replies
  • 0 kudos

ADC_Enable is timing out on STM32G031G8

I'm getting a timeout error when trying to configure a G031 to convert 8 channels. Any ideas what could be causing this? Here is the code: /* USER CODE BEGIN Header */ /** ***************************************************************************...

Pull resistor in I2C in STM32f334

I am using STM32f334 I2C as master and my slave is Arduino UNOMy problem is I am unable to receive anything from my masterI think the problem here is pull resistor, first I tried using Internal pull resistor but it did not work, then I tried with 2k ...

SADEP.1 by Associate
  • 1253 Views
  • 1 replies
  • 0 kudos

How to separate variables using MPU on STM32F429ZI?

This is kind of a broad question, but I'm having a bit of trouble understanding/finding resources on using the MPU on this MCU. My goal is to partition some of the variables in my code so that they cannot be accessed by accidental writes/overflow, an...

CMora.1 by Associate
  • 1905 Views
  • 2 replies
  • 0 kudos

Resolved! Why I cannot register for the STM32H5 webinar??

This is the first time that I cannot register with my usual email address (which I use for this community). Just have registered for another webinar on STM32MP. Why registration for the H5 webinar does not like my email? 

_legacyfs_online_stmicro_images_0693W00000bjUyYQAU.png
Pavel A. by Super User
  • 3189 Views
  • 8 replies
  • 0 kudos

Debugging from bank 2

I'm working with Nucleo-f439zi board.I use dual banking feature.I cannot find a way to debug from bank 2how to debug application from bank 2 ?

Is internal pull up the same as external pull up resistor.

for example IC2 needs pull up resistor on the board but there is internal pull up options for pins.I wonder if this is the same. So by setting internal pull up you can skip the pull up resistors on the board. I know that NRST pin has internal pull up...

_legacyfs_online_stmicro_images_0693W00000biJeBQAU.png
MNapi by Senior III
  • 7277 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.