Ask questions, find answers, and share insights on STM32 products and their technical features.
I notice that almost all peripherials return HAL_StatusTypeDef but GPIO not. Why?
Since when is STM32L152RE LQFP64 NRND?From the looks best pin compile etc. would be STM32L552RE is there any overview for doing this transition. Else I would need to do detail compare my self but as these MCUs seem to be in one line I was hoping ther...
Would need release dates for:L433 - guessing from searching around 2017L152 - guess 2015L552 - guess 2018L072 - guess 2016has anybody a way to find out or the data? Thanks a lot
when I press an external interrupt button, I want to switch to static IP, press again want to switch to DHCP, how can I get this? because in CubeMX it just defines once for LWIP_DHCP macro and how can I use this for static IP or vice versa ?
If I comment out the instantiation, compile and run, then uncomment the instantiation, compile and run, the code will work fine from that point on. But it will not run without hard faulting unless I do the comment / uncomment thing. Here's the code f...
I enabled WWDG on the MX and there were no other settings. MX_WWDG_Init(); As the function executes, the CPU resets, and when I look closely, I see that __HAL_RCC_WWDG_CLK_ENABLE(); As soon as the function runs, the CPU is reset. What should I do?Bel...
Hello,Didn't found a better way to ask this question elsewhere.I was registered to watch STM32 Innovation live on March 7, but I didn’t have enough time to watch it completely.I tried to register again on this page: content.st.com/stm32-innovation-li...
Hi everyone,I'm trying to transmit and receive data through rs485 with uart. Using Uart with DMA in normal mode and referance from this project. https://controllerstech.com/rs485-module-and-stm32/However, in this project there are 2 different stm. I ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.