STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo Board F746ZG, USART connection with ROS, issue: Unable to sync with device; possible link problem or link software version mismatch such as hydro rosserial_python with groovy Arduino

My Demo I need to establish a USART connection between my board and ROS1. The python code I run in ROS environment is in the package "rosserial_python" and it is called "serial_node.py". I followed this guide ( https://www.youtube.com/watch?v=cq0HmKr...

Italo by Associate II
  • 1908 Views
  • 1 replies
  • 0 kudos

An issue with event flag

Hello,I have an issue with event flag I am setting this flag inside ISR of GPIO pin interrupt and there is a task wait for this flag but even if the interrupt is come and set the event flag the task still in blocking mode this my code : void MXT_vidT...

rsoli.1 by Associate II
  • 1503 Views
  • 1 replies
  • 0 kudos

Why can't I clear the SRAM_PEF bit?

Hi there,I'm using the chip STM32G431CBY3 and here is a strange thing. After I start the TIM15 in interrupt mode and every time the interrupt enters, the NMI_Handler enters at the same time, by checking the register, I found that SRAM_PEF bit is set ...

jhu.51 by Associate
  • 1361 Views
  • 3 replies
  • 0 kudos

STM32H7A3 HAL_FLASH_Program() data and address alignment

Hello There,I'm working on an IAP application based on STM32H7A3 and have a query related to code alignment.Correct me if I'm wrong, as per my understanding HAL_FLASH_Program() in H7A3 writes a flash word (i,e., 16 Bytes) at a time. If so, then it mu...

KAgga.1 by Associate III
  • 4425 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.