STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! what is H5 IDAU configuration ?

I could not find yet a specific information regarding IDAU configuration of H5. Is it same as U5 as described in AN5347 ?Edit: I think it is the one in the reference manual (RM0481), I realized colors (Figure 2) indicate the IDAU mapping.

mete by Senior II
  • 1739 Views
  • 1 replies
  • 1 kudos

STM32G474RE Startup Issue

Hi everyone,I have a hardware problem with STM32G474RE on startup. If I try to supply this MCU directly from the lab power supply, it runs correctly, but when I have dips or drops or fast switching on the supply, I notice that the MCU doesn't start. ...

DKlew.1 by Associate
  • 1827 Views
  • 2 replies
  • 0 kudos

Echo cancellation on STM32F769I-DISCO

Hi, I need to perform a noise reduction and echo cancellation on an audio signal coming from an analog microphone and going out on a loudspeaker in order to make VOIP between 2 boards. I have an STM32F769I-DISCO board containing an STM32F769, a WM899...

PascalB by Associate
  • 2055 Views
  • 1 replies
  • 0 kudos

OV5640 Issue in JPEG mode

Hi,I try to use your OV5640 board with your OV5640 driver in STM32H747 BSP in JPEG mode.The problem is that the FPS drop to 1 or 2 even at low resolution QVGA.Can you show me what registers needed to be modified to make it work correct since your dri...

MSale.1 by Senior
  • 1951 Views
  • 1 replies
  • 0 kudos

STM32U575: pullup needed on NRST pin?

We have designed, build and assemble a board with a STM32U575OGY6QTR. The first tests went well with the ST-LINK/V2 programmer connected to the board (driving the NRST). Now we have removed the programmer, and under some circumstances the MCU does no...

tcachat by Associate II
  • 1776 Views
  • 1 replies
  • 0 kudos

Resolved! FIR-filter for STM32F4 and several frequency bands?

Hi,there are a lot of examples and tutorials available that describe how to use a FIR-filter (via function arm_fir_f32()). Unfortunately all these examples are either simple low-, high-, or bandpass-filters. Now what I'm looking for, is a possibility...

BSchm.6 by Associate III
  • 4894 Views
  • 4 replies
  • 1 kudos

Designing with STM32L496QGI6

Hello Team,We are planning to use the MCU STM32L496QGI6 for one of our new projects.The MCU will be powered from a 1.8V source (since all external peripherals are working in 1.8V only).One of the SPI slaves is working in 3.3V, so we are planning to u...

SVarg.2 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

Resolved! How can STM32F769 DMA controllers access the DTCM?

I am working with the STM32F769 microcontroller and I can see that a lot of DMA buffers are placed in DTCM in the source code I'm working with. Looking at the data sheet ( https://www.st.com/resource/en/datasheet/stm32f765bi.pdf ) page 20 I don't see...

arnold_w by Senior II
  • 2967 Views
  • 2 replies
  • 0 kudos

Stm32h7 HRtim input capture ability

Can I measure low pulse duration(>10ns) using the STM32H Hrtim?Hi all,I'm new to STM32H7 development. So I'm hoping to get some help to start.I need to measure pulse duration in 5- nanoseconds resolution or less. I then need to transfer the measured ...

Burakgvl by Associate II
  • 6398 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.