STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with CDC and FreeRTOS streams

I'm experiencing a weird race condition / hangup with an application that I've built for my STM32F407VGTx. Basically I connect to the device via a USB cable and open a terminal to type commands on the device like a CLI. Everything works fine until I ...

Screenshot 2023-09-14 at 8.21.27 PM.png
bdill.1 by Associate II
  • 1433 Views
  • 0 replies
  • 0 kudos

STM32U575 - USBPD_CAD_Init error wit Thread-Safe setting

Hello,I am building an application using ThreadX, FileX, USBX and USBPD. Everyting runs perfectly until I bring USBPD in the game. Whatever I do, I always get an error when the library calls USBPD_CAD_Init().More precisely, the function fails at a ca...

Pepils by Associate II
  • 4308 Views
  • 5 replies
  • 0 kudos

Regarding STSW-IMG010

Hi, I have  X-NUCLEO-53L0A1 and X-NUCLEO-53L5A1 board can any of these boards be used to run the STSW-IMG010. The documentation in STSW-IMG010 mentions that we should use a X-NUCLEO-53L1A1. Please let me know if I should make any modifications to mak...

Update/re-program STM32F722 Firmware via UART

Hello everyone,I have a project where I use a main baseboard that connects to an STM32F722 microcontroller via a UART interface. My goal is to achieve updating the program running on the STM32F722 without requiring any user intervention. In other wor...

Juanjo97 by Associate II
  • 13283 Views
  • 7 replies
  • 0 kudos

Programing firmware

I am developing a board using the STM32H725. We are currently programing each board using the STM32Cube    programmer and then we send the PCB on a test bench to test each card. This step that seems to be quite simple but it actually adds additional ...

josimmor by Associate
  • 4100 Views
  • 2 replies
  • 1 kudos

ADC noise on STM32F413

Hello,For a project (control motor application), we are using ADC from MCU STM32F413. We encounter some noise on ADC measurments. We observe to high standard deviation on our ADC result.We show in errata doc of mcu  we an issue: "Internal noise impac...

AlexisC by Associate II
  • 4868 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.