STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 as a SPI slave data transmit error

hi there, I want to communicate between two Stm32 using SPI, when i transmit date from master to slave, it received(using received interrupt). but when want to transmit date from slave side it gives HAL_error,master side code while (1) { for(int...

ykn by Senior
  • 2748 Views
  • 2 replies
  • 0 kudos

Resolved! About filter behavior in case of ID list and 16bit scale

HiI would like to know about filter behavior in ID list mode and 16bit scale.I would like to receive 3 standard IDs.I know that with the combination of ID list and 16bit scale, I can receive 4 standard IDs. In this case, one will remain when setting ...

Ukazu by Associate III
  • 2592 Views
  • 4 replies
  • 0 kudos

USB ISTR IDN and USB CHEPxR EA fields

RM0481 says: (I am using STM32H563)USB_ISTR.IDN is the endpoint (or channel in host mode) identification number that generated the interrupt request, and if there are more than one endpoint requesting an interrupt, the lowest (CHEP0R) has a higher pr...

mete by Senior II
  • 921 Views
  • 0 replies
  • 0 kudos

can protocol error

This is a question I posted on Reddit a long time ago, but it hasn't been solved yet, so I'm asking here.I solved the dlc value in the notepad picture.And there was an error even though I connected the rs pin afterwards.I want to know the solution to...

jha g.1 by Associate
  • 2966 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H573VI ETH_TXD1 and ETH_TX_EN pins

Hi,When using the STM32CubeMX to configure the ethernet pins for the STM32H573VI, the TXD1 and TX_EN pins can be configured to the PB13 and PB14 pins. But the STM32CubeMX does not allow these pins to be configured for ethernet for the STM32H563VI. In...

Asantos by Senior
  • 2466 Views
  • 2 replies
  • 0 kudos

DISABLE/ENABLE EXTI interrupts using hal

Posted on November 10, 2015 at 15:39Hi, I need to disable a EXTI interrupt and then enabling it again later. How can I do that using the hal implementation? I am working on STM32F070.

seed by Associate III
  • 11337 Views
  • 4 replies
  • 3 kudos

Resolved! stm32f103c8 classB

hello, I am applying the safety library provided by st company to stm32f103c8.In the example provided, the capture function of TIM5 is connected to the LSI oscillator, but the MCU (stm32f103c8) I use does not seem to be able to connect to the LSI osc...

jihoon by Associate II
  • 5721 Views
  • 9 replies
  • 5 kudos

STM32F412VG - CAN SCE Interrupt problem

Hi,I have a problem in my program with the CAN SCE Interrupt. I work with a STM32F412VG but I have the same problem with a STM32F413VG, STM32F103C8 and STM32F042K6. And I work with MikroPascal Pro IDE from MikroElektronika.I try to get an interrupt w...

RCLER.1 by Associate
  • 2163 Views
  • 1 replies
  • 0 kudos

Resolved! DMA transfer delay when EXTI occur

My target:I want to use the same uart lines(RX line and TX line) to achieve communication between computers and multiple devices (in other words: multiple slave devices, computer as master). I use some STM32F072C8 as slave devices, and configure thes...

pic.png
way by Associate II
  • 1775 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.