STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to reduce power consumption while connected via CDC USB

I'm developing a board with an STM32L452 and would like to find out if I can improve power consumption while it remains connected via USB (as a device). I've tried putting the device to sleep using the following code: while (1) { // ... do stuff HA...

antfarmer by Associate III
  • 7084 Views
  • 10 replies
  • 4 kudos

Sending message from slave to master (SPI)

Hello,I'm trying to send a message from slave to master using spi (I'm using only one stm board) and so far nothing I tried has worked. AFAIK for the slave to send data to master, the master has to initiate communication first by sending clock signal...

Jordalic by Associate II
  • 5476 Views
  • 4 replies
  • 0 kudos

Unable to access QuadSPI Flash 2 with stm32h747i

Hi im currently using STM32H747I EVK board and working on QSPI ,im able to perform all the QSPI operations in FLASH1 but when u configure it as the FLASH2 nothing works . static void MX_QUADSPI_Init(void){ /* USER CODE BEGIN QUADSPI_Init 0 */ /* USER...

SPI + I2C Example Project

Hi, I am struggling to get SPI and I2C to work at the same time on my project I have tried multiple things (DMA, interrupts etc...) are there any example projects that already have this implemented? I am simply trying to read an I2C sensor value and ...

Linkpad by Associate III
  • 2392 Views
  • 3 replies
  • 2 kudos

Problem using Slave to transmit I2C Interrupt

Hi,In my project, I communicate with STM slave I2C. I can receive data via I2C but I cannot send data. As you can see in the photo below, the packetData is filling up, but when you send it, it only sends 0x00. what is the problem? what can I do?

i2c-interrupt.PNG i2c-interrupt-2.PNG
res_queen by Associate II
  • 2619 Views
  • 4 replies
  • 0 kudos

Resolved! Transition from 2x Teensy 4.0 boards to STM32H755xI

Hello everyone,  I'm exploring the feasibility of transitioning from 2x Teensy 4.0 boards to an STM32H755XI for a sensor-intensive application. The project involves interfacing with 16 VL53L4CX sensors and managing their data acquisition and processi...

isaacjack by Associate II
  • 2601 Views
  • 1 replies
  • 1 kudos

SMT32F407VGT6 / CAN issue

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! I...

JACK00 by Associate II
  • 1475 Views
  • 1 replies
  • 1 kudos

STM32F407 USB OTG_FS - OTG_FS_GRXSTSR register invalid

I'm working on implementing USB Host support for the STM32F407 without using the STM32 HAL. I've followed the datasheet and gotten as far as sending a GetDescriptor packet (though I haven't confirmed that on the logic analyzer yet), but I don't know ...

dbristow by Associate
  • 1481 Views
  • 1 replies
  • 0 kudos

STM32F303C8C6 DMA 2ADC 5Channels

hi i am having some difficoulty's where i cant find a solve for: problem 1 ADC1_channel12 feeds me a value back around 4030 while its voltage on the pin is 0.0Vproblem 2 ADC2_channel3 is always reading 0 i configured all ADC channels to place data in...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.