STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Turning ON LED on Nucle-G474RE not working when not using HAL

Hi.I am learning how to turn on LED2 of a NUCLEO-G474RE board by using registers (without HAL).I have created a small project which contains:    // This first block works and updates the registers // Start GPIOA Clock (*(uint32_t*)0x4002104C) &= ~(1 ...

RPG by Senior
  • 5602 Views
  • 9 replies
  • 2 kudos

Resolved! STOP mode in STM32F103

I'm looking for the low power function of the STM32F103TB. I have some questions about this function:1. I read the code of the AN2629, there has no interrupt routine code. So when we use the RTC alarm and the PA0 (wake-up pin) to wake up the MCU, whe...

HF.Wang by Associate II
  • 3173 Views
  • 1 replies
  • 0 kudos

HAL_I2C_ErrorCallback occurred randomly in I2C communication

Hi, Currently, we are working with STM32L476JGY6TR MCU. We are facing HAL_I2C_ErrorCallback - 0x00000004 error randomly while communicating with MCU.  We are communicating with the MCU Frequently with particular time intervals. In this scenario, some...

ArunyaS by Associate II
  • 2978 Views
  • 3 replies
  • 0 kudos

Resolved! F411 Nucleo Board ADC Issues

I tried to use ADC in F411 to read two ADC inputs.My hardware is a F411-Nucleo board; my IDE is CubeIDE.The followings are my ADC settings in IDE:                                 I use 2 channels in ADC1 (IN1, IN4)I also use DMA to obtain ADC results...

Setting_1.PNG Setting_2.PNG Setting_3.PNG
HDaji.1 by Senior
  • 2709 Views
  • 3 replies
  • 0 kudos

Resolved! enter/exit STOP mode with one GPIO pin

Hello everybody,I want to use the STM32F042G6U6 MCU with one button on PA6 pin if I press the button it should toggle between STOP mode and run. Is this possible at all?How can I do this? I was able to enter STOP mode or exit from it but I cant toggl...

DMA to BSRR Transfer - single signal error

Hello! I am using the STM32F446RE Nucleo Board and succeeded in sending a signal chain via DMA to the GPIO Bank B, i.e. the BSRR register.  The DMA trigger works very fine. However, one of the 8 signals is missing/not generated/skipped... This is whe...

Resolved! STM32F4 - Timer - Max Frequency External Clock Source ETR

Hi,We have a custom firmware running in an STM32F427, and I'd like to find out what the highest frequency supported on a timer with an external clock source using ETR function.Based on AN4776, I can use a prescaler function (ETR) to read clock freque...

RNJ by Associate II
  • 8375 Views
  • 8 replies
  • 6 kudos

Resolved! Help choosing the best external RAM for STM32H723

Hi all!I am making a PCB with STM32H723, and have chosen this MCU due to its greats specs and versatility. However I would like to add at least 4Mbit (0.5MB) of RAM, either as SDRAM, SRAM or PSRAM etc. using the FMC (Flexible memory controller). Howe...

elso by Senior
  • 6481 Views
  • 1 replies
  • 1 kudos

Resolved! CAN ExtID filter for exactly two IDs

Dear Community, even after reading what feels like 100 posts, I still can't manage to set the filter so that exclusively 2 IDs are let through.I use the extendet ID, 1 Byte IDs and have managed to let exactly one ID through with the MASK_MODE, as you...

Anno by Associate II
  • 6313 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.