2015-07-20 8:49 AM
Hello,
i'm using a STM32F334C8 with STM32CubeMx and with Atollic True Studio or SW4STM32.When i generate a project with STM32CubeMx (for TrueStudio or SW4STM32) the linker file is wrong. I get a 16ko size ram instead of 12ko. When i try to debug, an address error occurs. I have to manually modify the linker file (*.ld) and after everything is ok.When i create a project with True Studio only, the linker file is ok.This is very strange. Is it a bug or do i miss something ?Thanks2015-08-27 10:41 AM
Dear user,
These are known issues. Please upgrade to next Cube MX 4.10 when it is released next week. Best regards2015-08-31 1:16 AM
2015-09-01 7:08 AM
Dear user,
You are correct. The issue has been logged. Thank you for your feedback.2016-02-09 3:05 AM
Dear user,
The issue is now fixed in STM32CubeMX 4.13.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.