2014-05-05 1:36 PM
Hello Everybody,
in the process of compiling some of the Examples for the STM32F429DISCO on a linux machine I noticed that Include paths are specified using backslashes instead of slashes. Obviously, backslashes only work on Windows and I had to modify the BSP to use Slashes to make it Compile on linux. Quote from K&R (via https://code.google.com/p/tageventor/wiki/pcscHeaders) The characters in the name filename must not include > or newline, and the effect is undefined if it contains any of '', ', \, or /. I'd appreciate if future Releases of the CubeMX software package used slashes for path separation. Slashes work on Windows, too. Lukas2014-05-09 1:42 AM
Hi Lukas,
Can you please provide a file as example. Thank you.2014-05-13 11:47 AM
Hi there,
take a look at the file ''Drivers/BSP/STM32F429I-Discovery/stm32f429i_discovery_lcd.c'' #include ''..\..\..\Utilities\Fonts\fonts.h'' This line (and all the others) should read like that #include ''../../../Utilities/Fonts/fonts.h'' this way, it works on all operating systems.2014-05-14 9:45 AM
Hi lukas,
I'm wondering with which compiler are you working on the linux machine ?With regards.2014-05-14 11:50 AM
I guess that goes to K&R's undefined behaviour.
I did confirm back when you originally posted that Keil uV 4.7x was tolerant of slashes in either direction. I don't know that's true for all C compilers, I'm sure the DOS/Windows compilers stumble over this format more frequently than the other way round, but tolerance is a two-way street, perhaps the Unix compilers should work either way too.2014-05-15 8:54 AM
I'm using the GCC (also used by Attolic True Studio)
Concerning compilers not accepting slashes as path separators: That's not (or should not be) the compiler's business. The Compiler will pass the path to the Operating system. http://en.wikipedia.org/wiki/Path_%28computing%29#MS-DOS.2FMicrosoft_Windows_style Windows accepts both slashes and backslashes. The STM32Cube package even contains Source files using #includes with slashes as path separators. (in LwIP, fatfs, freertos)2014-05-17 7:56 AM
Hi, i'm using stm32F429 and i and to display a variable which increment from 1 to 5 but it didn't work can please help me.This is the code
#include ''main.h''void Delay(unsigned long period) { unsigned long j; for(j=0;j<=period;j++);} int main(void){ uint8_t i; /* LCD initiatization */ LCD_Init(); /* LCD Layer initiatization */ LCD_LayerInit(); /* Enable the LTDC */ LTDC_Cmd(ENABLE); /* Set LCD foreground layer */ LCD_SetLayer(LCD_FOREGROUND_LAYER); LCD_Clear(LCD_COLOR_WHITE); for(i=0;i<=5;i++) { LCD_DisplayStringLine(LINE(8), (uint8_t*)i); Delay(3000000L); }}#ifdef USE_FULL_ASSERT/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { }}#endif/** * @} */ /** * @} */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/2014-05-23 8:49 AM
Hi Rihab,
Please write a new forum post describing your problem.With regards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.