2025-07-10 12:03 AM
Hello,
I am trying to implement an edge AI application on the B-U585I-IOT02A board alternating between active mode for inference and stop2 mode. I based the implementation on the PWR_LPMODE_RTC example for the U575 board, I have attached main.c below.
I am using Power Profiler Kit II in source meter mode to measure energy consumption. I have disabled ST-LINK via the SWD MCU switch. I power the board with 3.3V using the 3V3 pin through PPKII. I left the jumper at 5V_USB_STLK and I am using the default values in PPKII. During measurements, I observe a current of approx. 100mA in active mode and 80mA (instead of a few μΑ) in stop2 mode. I wanted to check whether:
Thank you!
2025-07-14 12:31 AM
Hello all,
I still can't make the current consumption during stop2 mode on the B-U585I-IOT02A SoC go below ~80mA. I've reviewed the configuration (RTC wakeup, WFI, clocks, etc.), and I'm increasingly leaning toward non-MCU components being responsible for the high current. I have confirmed the MCU enters STOP2, but the current barely drops from active mode (~100mA) to STOP2 (~80mA), which seems way too high for STM32U5 alone.
Would using the Nucleo U575 be a solution? Or measuring directly the MCU consumption through JP3 (I am not even sure this is possible, haven't tried yet)? Or is there something else that I am currently missing to turn energy consumption down?
Thank you very much!
2025-07-14 12:38 AM
The B-U585I-IOT02A may have high power consumption due to active peripherals or misconfigured low-power settings. Check clocks, GPIO states, and disable unused modules.
2025-07-14 1:39 AM
@jacks004 I am only enabling GPIO port H6/7 and clocks (if you see from the attached source files) and have also disabled RT-LINK through the relevant hardware switch. I am not explicitly disabling the rest of the on-board ICs, including BLE and WiFi but shouldn't they be set to off by default?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.