2019-10-29 10:04 AM
HI
I am newbie and just got my hands on STM32 Discovery Kit IoT Node.
According to the documentation the initial WiFi configuration was working fine. I was able to connect to WiFi. As i started playing around with it on STM32CubeIDE i have flashed various programs. Now, how to erase all ran programs and start with default WiFi program as it does for the first time.
2019-10-29 10:32 AM
I supposed you'd reflash it with the image of the firmware that it originally shipped with, and you'd saved with the ST-LINK Utilities or STM32 Cube Programmer beforehand?
Not a magic button I'm afraid.
STM32Cube_FW_L4_V1.14.0\Projects\B-L475E-IOT01A\Demonstrations\readme.txt
/**
@page AWS AWS Cloud demonstration
@verbatim
******************************************************************************
* @file readme.txt
* @author MCD Application Team
* @brief Description of AWS Cloud demonstration.
******************************************************************************
*
* Copyright (c) 2019 STMicroelectronics International N.V. All rights reserved.
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
@endverbatim
@par Demonstration description
The B-L475E-IOT01A board embedded demonstration is available in source code under
https://www.st.com/en/embedded-software/x-cube-aws.html
You can possibly upload your board with a more recent software version using this link.
This package starts with a STM32CubeExpansion_Cloud_AWS_VX.Y.Z directory.
STM32CubeExpansion_Cloud_AWS_VX.Y.Z\Projects\B-L475E-IOT01A\Applications\Cloud\AWS\readme.txt
will provide you with the details of the embedded demonstration.
It implements an Amazon AWS Cloud IoT client for the B-L475E-IOT01 board using
the on-board Inventek ISM43362 Wi-Fi module connectivity, and mbedTLS for secure
network communication.
The application connects to Amazon AWS IoT Cloud with the credentials provided
by the user. When the User button is pushed, it sends a LED toggle command to the
IoT Cloud endpoint, which returns back the message to the board and trigs the LED toggle.
The board sensor data are also collected and published to the cloud.
* <h3><center>© COPYRIGHT STMicroelectronics</center></h3>
*/
2019-10-30 7:10 AM
Thanks. Understood. I did not have the original file systems which it was originally shipped with, however i was able to run the sample mqtt example from
X-CUBE-CLD-GEN package.
2023-10-15 8:58 AM
Can you please provide me with configuration documents to connect to Wifi?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.