2018-06-03 9:46 AM
Dear STM32 Community,
I have a B-L072-ZLRWAN1 that I have programmed using arduino and the libraries from
. I use the board to connect to The Things Network and it works, as long as it is connected to my PC. However, if I try to power the board via the battery compartment, only LED 7 lights up but no connection to TTN happens. Any ideas what the reason could be? I am new to this board and couldn't find a solution in the specs. Thank you for your help and time!2018-06-03 10:01 PM
can you check the batteries voltage ? are they new or old batteries ?
did you check the reference manual, what voltage do you need ?
sometimes the battery's terminals corrode, check with a meter the battery voltage on the pcb wire connection.
2018-06-04 12:48 AM
Hi TJ, thank you for your quick reply.
The batteries were all new when I first tested, my multimeter reads ~1.482 V for each. As mentioned before, LD 07 on the board is lit up, which supposedly means +5V power is present. I tested the 3V3 Pin and got ~3.3V, for the 5V pin I got a reading of ~4.2V.The manual ( ) states that 3 x AAA Batteries are to be used (p. 14).There's nothing connected to the Board except for the standard antenna.
2018-06-04 12:55 AM
as a transmitter, it will need some capacity in those batteries, not just surface voltage that is already low.
you are out of luck, I only have 2 AAA's here, can't test it easily here.
the boards works on 5V USB Yes ?
did you try new batteries ?
2018-06-04 2:39 AM
I will try brand new batteries later today , although I am fairly certain that the ones I used were fresh from a recently bought pack when I started testing.
- The board correctly connects to TTN when I plug it into my computer via USB.
- It does not connect at all using batteries.
- I haven't extensively tested using USB solely as power source (eg via power bank or wall outlet) , however so far that doesn't seem to work either.
I wonder if I have to change anything on the board, but my understanding of the electronics involved is limited. I appreciate your help greatly!
2018-07-05 4:24 AM
I got a great solution from someone on github. Simply put a jumper between NRST and 3V3, that suffices. The jumper needs to be removed if you don't want to power the board with batteries any longer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.