2023-06-06 1:53 PM
Hello,
My question is about language C.
My nucleo receive some AT Command (from my pc) and i have write a function for compute the command.
Ex : AT+SPEED? > return "SPEED" (only).
>I 'm able to get only the command (by print over uart).
>My command is store inside a array.
command [0] = S
command [1] = P
...
Now a need to return this "value" from my function to another. One way is to convert this array into a string with atoi() function.
//------------------------------------------
return data =atoi(command);
//------------------------------------------
uint16_t Array[10];
sprintf( Array, "%c",command_value) ;
HAL_UART_Transmit(&huart1, Array, strlen(Array), 100);
it doesn't work, i mean no print.
I think is not a STM32 problem but a C problem.
Someone have an idea ?
2023-06-06 2:25 PM
>>sprintf( Array, "%c",command_value) ;
command_value is what?
you are printing as a character?
command [0] = 'S'; // as a character
command needs to be NUL terminated
atoi() needs to process a string containing a number, ie "123" not "SPEED"
Consider learning C on a PC platform, then move to embedded.
2023-06-07 5:38 AM
You have right, my problem is not a bug from STM32 but a C acknowledge issue.
I'm not a complete newbie and i have all documentation next me... the transition from theory to practice is not always easy.
My data is store like that :
uint8_t command[10]={0};where command[0] = 'S' / command[1] = 'P' / ...
i have write this following lines :
uint8_t data;
data = atoi(command);
uint8_t str[10];
sprintf(str, "\r\n %u", data);
HAL_UART_Transmit(&huart1, (uint8_t*)str, strlen(str), 100);the result is '0' in my terminal.
2023-06-07 6:29 AM
atoi() convert string to integer. For example atoi("193") is converted as integer value 193.
2023-06-07 11:03 AM
Hello
If you allready have this answer-string in command-array, you can send it directly:
HAL_UART_Transmit(&huart1, command, strlen(command), 100);Or if you need to add Line feed /carriage return in the beginning (which is bit odd, usually it is in the end), you can do like this:
uint8_t str[20];
sprintf(str, "\r\n %s", command);
HAL_UART_Transmit(&huart1, str, strlen(str), 100);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.