2012-12-23 1:30 AM
Hello.
I try to put a 32 bit word in the FLASH section which need to get know value at programming and during the program it can be modify. In this way I can know next time I power up that this varible has beed update.I use the IAR ARM 6.4.I modify the link icf file this way:/*♯♯&sharpICF♯♯♯ Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*//* IcfEditorFile=''$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml'' *//*-Specials-*/define symbol __ICFEDIT_intvec_start__ = 0x08000000;/*-Memory Regions-*/define symbol __ICFEDIT_region_CONSTANT_start__ = 0x08004000;// change by Bar for placing constant in the FLASHdefine symbol __ICFEDIT_region_CONSTANT_end__ = 0x0800BFFF; // change by Bar for placing constant in the FLASHdefine symbol __ICFEDIT_region_ROM1_start__ = 0x08000000; // for BOOTLOADERdefine symbol __ICFEDIT_region_ROM1_end__ = 0x08003FFF; // for BOOTLOADERdefine symbol __ICFEDIT_region_ROM2_start__ = 0x0800C000;define symbol __ICFEDIT_region_ROM2_end__ = 0x080FFFFF;define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;define symbol __ICFEDIT_region_RAM_end__ = 0x20020000;/*-Sizes-*/define symbol __ICFEDIT_size_cstack__ = 0x400;define symbol __ICFEDIT_size_heap__ = 0x200;/**** End of ICF editor section. ♯♯&sharpICF♯♯♯*/define memory mem with size = 4G;define region ROM1_region = mem:[from __ICFEDIT_region_ROM2_start__ to __ICFEDIT_region_ROM2_end__] ; //-mem:[from __ICFEDIT_region_ROM1_start__ to __ICFEDIT_region_ROM1_end__];define region VECTOR_region =mem:[from __ICFEDIT_region_ROM1_start__ to __ICFEDIT_region_ROM1_end__];define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];define region CONSTANT = mem:[from __ICFEDIT_region_CONSTANT_start__ to __ICFEDIT_region_CONSTANT_end__ ];define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };initialize by copy { readwrite };do not initialize { section .noinit };//place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };place in CONSTANT {section .noinit};place in ROM1_region { readonly };place in VECTOR_region { readonly section .intvec };place in RAM_region { readwrite, block CSTACK, block HEAP };The idea is to leave the first section for startup and the bootloader, the second one for modify variable , the third for fix data like version ect. and from the 4th to the code.And in the main file I write at the top before the main this:/* Sector 1, 16 Kbytes */
/* the last know MCU Baud Rate */
&sharppragma location=0x08004000
__no_init volatile uint32_t Baud_Rate_USART=0;
I have 2 problems about it.I can't see in the memory windows the FLASH area. Is it possible from the view menu?I see that for FLASH assign I need to write no_init. SO how I can give it perleminary values because i see it doesn't?RegardsBar. #variable-assign-to-flash2012-12-23 5:52 AM
Well, you're not going to want to use noinit if you expect a value to be set.
The most sensible solution is to have code to identify the uninitialized state and to write default values. You could also write specific/calibration values during a final test procedure on the board. Placing all this in configuration structure, with a signature and checksum, is also something to consider. I'd probably use ''const'' or ''static const'' to define at variable at a specific location, but modified outside of normal C functionality (ie a simple write is not possible)const int baud @ 0x08004000 = 9600;
http://supp.iar.com/Support/?note=36121
2012-12-23 8:06 AM
Thanks for the answer.
I solve the init problem.But I have anther problem.Also I have define a special place for the CONSTANT from 0x08004000 to 0x0800BFFF.and the start up code from 0x08000000 to 0x08004000and the code I ask to start from 0x0800C000 to 0x080FFFFFhere is the setting in link icf/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*//* IcfEditorFile=''$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml'' *//*-Specials-*/define symbol __ICFEDIT_intvec_start__ = 0x08000000;/*-Memory Regions-*/define symbol __ICFEDIT_region_CONSTANT_start__ = 0x08004000;// change by Bar for placing constant in the FLASHdefine symbol __ICFEDIT_region_CONSTANT_end__ = 0x0800BFFF; // change by Bar for placing constant in the FLASHdefine symbol __ICFEDIT_region_ROM1_start__ = 0x08000000; // for BOOTLOADERdefine symbol __ICFEDIT_region_ROM1_end__ = 0x08003FFF; // for BOOTLOADERdefine symbol __ICFEDIT_region_ROM2_start__ = 0x0800C000;define symbol __ICFEDIT_region_ROM2_end__ = 0x080FFFFF;define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;define symbol __ICFEDIT_region_RAM_end__ = 0x20020000;/*-Sizes-*/define symbol __ICFEDIT_size_cstack__ = 0x400;define symbol __ICFEDIT_size_heap__ = 0x200;/**** End of ICF editor section. ###ICF###*/define memory mem with size = 4G;define region ROM1_region = mem:[from __ICFEDIT_region_ROM2_start__ to __ICFEDIT_region_ROM2_end__] ; //-mem:[from __ICFEDIT_region_ROM1_start__ to __ICFEDIT_region_ROM1_end__];define region VECTOR_region =mem:[from __ICFEDIT_region_ROM1_start__ to __ICFEDIT_region_ROM1_end__];define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];define region CONSTANT = mem:[from __ICFEDIT_region_CONSTANT_start__ to __ICFEDIT_region_CONSTANT_end__ ];define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };initialize by copy { readwrite };do not initialize { section .noinit };place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };place in CONSTANT {readonly section .data_init};place in ROM1_region { readonly };place in VECTOR_region { readonly section .cstart };place in RAM_region { readwrite, block CSTACK, block HEAP };I don't get it in the Memory map.Attach the start of the map where you can see the reset vector start on 0x08000000 but immediate after it the code is writing.''A1'': place at 0x08000000 { ro section .intvec };
''P1'': place in [from 0x08000000 to 0x080fffff] { ro };''P2'': place in [from 0x20000000 to 0x20020000] { rw, block CSTACK, block HEAP }; Section Kind Address Size Object ------- ---- ------- ---- ------''A1'': 0x184 .intvec ro code 0x08000000 0x184 startup_stm32f2xx.o [1] - 0x08000184 0x184''P1'': 0x478c .text ro code 0x08000184 0x115c APP_handle_main.o [1] .text ro code 0x080012e0 0x1fc TIM_APP_handle.o [1] .text ro code 0x080014dc 0x7f8 ADC_DMA_APP_handle.o [1]Where I wrong in the link icf file and what can be done to fix it?RegardsBar.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.