2018-11-26 8:43 AM
2018-11-26 9:29 AM
>>Anyone help me ?
Probably not with CubeMX, isn't that a point and click interface?
This is a Master/Slave SPI demo program using HAL
STM32Cube_FW_F1_V1.6.1\Projects\STM32VL-Discovery\Examples\SPI\SPI_FullDuplex_ComPolling\readme.txt
2018-12-03 7:53 PM
Yes i am using cubemx and i try code from stm32cubef1 but I don't get any result. Can you help me further ?
2018-12-03 8:03 PM
Start by being more specific about your board/hardware.
Define which pins you are using.
Start with the Master, send continuous patterns and review signals with a scope or analyzer.
#ShowYourWork
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.