2018-08-30 7:40 PM
I am a bit confused with this setup but hopefully someone can enlighten me with the correct approach, I have an MCU based system and I need an LCD, unfortunately, it needs TFT controller thats why I add STM32F746 in the middle. hope someone can correct me, thanks
2018-08-30 9:39 PM
What size/resolution are we talking about?
What are you attempting to make the panel do? Text, bitmaps, menus, line drawing?
Is this a commercial project?
2018-08-30 11:05 PM
this is a concept project,
basically, the setup is I want to display something on my lcd tft, for me to do that, do I need to send command from spi mcu to spi stm32f746 to display something on the screen?
this spi commands, do stm32f746 provide these commands?
thanks
2018-09-02 7:13 PM
I think my understanding with this setup is wrong
thank you for taking time to review my problem, will close this
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.