2016-03-21 9:25 AM
We have a batch of boards in the field where the LSE crystal may be marginal and I'm wondering if there's a way to check for the LSE losing lock after initially being locked. That is, if on initial clock setup I get a positive response from RCC_GetFlagStatus(RCC_FLAG_LSERDY), but later the LSE stops.
I've looked at the RCC_BDCR register and it doesn't seem to change, even if I short out the crystal, but I do see the RTC stop advancing.So is my only option to check for the RTC stopping advancing and use that to flag a problem ? Thanks in advance2016-03-21 9:45 AM
> I've looked at the RCC_BDCR register and it doesn't seem to change, even if I short out the crystal, but I do see the RTC stop advancing.
Yes, unfortunately LSE_RDY flag does not seem to reflect the true state of LSE, serving only as a startup indicator. I guess it's just an output from a saturated fixed-count counter fed by LSE. Some newer STM32 models (e.g. 'L0, I did not check elsewhere) feature a LSE-CSS, but not the 'F2/'F4. You might perhaps want to check out the 'L4. RTC output event may be fed into TIM5_CH4, see TIM5_OR, but I don't know exactly could that be used for any automatism to check LSE running. JW2016-03-21 9:55 AM
If you use the SysTick timer as a timebase, for example in an RTOS, and you generate a 1 second t interrupt from the RTC, then if you get 2 seconds worth of SysTicks but no RTC you can conclude the LSE failed.
I also reset the IWDG from the 1 second RTC since an LSE failure is a fatal event in my applications. After a reset if you see the IWDG as the source you know the RTC isn't working and can fall back to the LSI as a workaround.2016-03-21 11:26 AM
Thanks guys. I'll use the SysTick interrupt to monitor the RTC and restart it on the LSI if I notice a loss of ticking. That will suffice for almost all functionality.
2016-03-21 12:30 PM
RTC output event may be fed into TIM5_CH4, see TIM5_OR, but I don't know exactly could that be used for any automatism to check LSE running.
You can use it to measure the period, or up to 8 periods, of the LSI, or LSE. In a 1ms ticker, you'd expect this timestamp (in TIM5->CCR4) to precess.2016-03-21 2:11 PM
By ''automatism'' I meant ''no stinkin' software-checking-periodically, just interrupt me when the clock stops''. Should that channel be CH1 or CH2, I'd tie it to the slave controller and reset the timer from RTC; then set another channel to interrupt just beyond the one second mark. Maybe something similar could be accomplished by employing a DMA triggered by CH4, writing a well-chosen constant to some of the timer's registers.
JW2025-04-11 3:14 AM
So How do we detect that LSE is Working or not?
2025-04-11 3:18 AM
The OP said, "I do see the RTC stop advancing" - so use that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.