2016-05-01 11:34 PM
Hi,
in chapter 1.1.4 of AN4661 is descriped that if DSI is not used at all then: ''The VDDDSI pin must be connected to global VDD'' There is also written: ''The VDDDSI pin must be grounded.'' Is this a typo? What is correct? Both requirements do not make sence together.2016-05-02 3:28 AM
Hi neumann.sascha,
Thank you for bringing this feedback to us. Here is a correction for this point:
“
If the DSI functionality is not used at all, then:
• The VDDDSI pin must be connected to global VDD.
• The VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
• The VSSDSI pin must be grounded.
“
Sorry for the inconvenience.
-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.