2021-03-08 8:33 PM
i configure tim1 bkin. after bkin is triggered, tim1 2 3 output seems like high-z state.
my ossi bit is 0. MOE is cleared by trigger. according to reference i can set corresponding GPIO to high or low. but it doesn't work.
2021-03-12 1:19 AM
Hi @rpip.1 ,
Which product are you using?
Besides to the reference manual, there is an application note which explains the break feature and provides examples for various possible configurations.
It is AN4277: Using STM32 device PWM shut-down features for motor control and digital power conversion.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.