2013-09-04 12:37 PM
Hi,
For my project I need additional RAM, is it possible to add memory to the STM32F407VG (in the STM32F4-Discovery Board) using the FSMC interface?2013-09-04 12:58 PM
Review schematics and pin allocations for boards using external memory, like STM3240G-EVAL or RedDragon407
Look also for daughter boards which you can plug the STM32F4-Discovery into. Personally I'd be looking for a different board, with a higher pin count STM32 part to better accommodate the DCMI and FSMC interfaces. Check eBay, etc.2013-09-04 1:19 PM
Thanks for your answer CLIVE1.
In the STM32F4-Eval board we have only 8 address outputs (A16 to A23). What can be the maximum memory they could controle? Can it reach 16MB?2013-09-04 2:24 PM
About 256 or 512 bytes depending on if your data bus is 8 or 16-bit wide?
I haven't looked at the STM32F4-Discovery being a practical platform for external memory, depending on the memory you'd have to wire up ~30 pins. The camera would be another ~20 pinsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.