2019-05-04 3:52 PM
Hello All
I have configured ADC1 and ADC2, each with CONT=1 and L = 0, to convert two respective analog inputs on a software start, and the scheme works fine. However, when in the CCR I set the MULTI bits to 0b00110 (or to anything else for that matter), no non-zero data appears in the CDR. I know this as I send the read to an analog output and watch it on the scope.
Any ideas? All I need is to make sure that the two analog channels are sampled simultaneously and continuously following a software start. Is there anything involved other than setting the MULTI bits and reading the data from CDR as opposed to from the two DRs?
Much appreciated
Amir
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.