2018-06-18 2:04 AM
Hello,
as there is no DMA2 on the STM32F334, the SYSCFG->CFGR3 Bit 9 ADC2_DMA_RMP[1] has a misleading description. Following the description, is has to be kept set. 10.1.8 SYSCFG configuration register 3 (SYSCFG_CFGR3) is also missing Address offset and System reset value.
2018-06-19 2:20 AM
Hello
Bonnes.Uwe
,You are right, the description will be changed to:
Bit 9 ADC2_DMA_RMP[1]: ADC2 DMA controller remapping bit
0: Reserved
1: ADC2 mapped on DMA1
We will add the
missing Address offset and System reset value:
Address offset:
0x50
System reset value:
0x200
This is
rasied internally for update in the coming release of the reference manual RM0
With Regards,
Imen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.