2014-01-27 11:13 PM
Guys,
Am I right on initializing ADC ? It's running only one time and then freeze, I put it on forever loop, but stopping, never looping again, any wrong configuration here ? thanks //read internal temperature sensor begin RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); //ADC1 configuration //select independent conversion mode (single) ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; //We will convert single channel only ADC_InitStructure.ADC_ScanConvMode = DISABLE; //we will convert one time ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; //select no external triggering ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; //right 12-bit data alignment in ADC data register ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; //single channel conversion ADC_InitStructure.ADC_NbrOfChannel = 1; //load structure values to control and status registers ADC_Init(ADC1, &ADC_InitStructure); //wake up temperature sensor ADC_TempSensorVrefintCmd(ENABLE); //ADC1 channel16 configuration //we select 41.5 cycles conversion for channel16 //and rank=1 which doesn't matter in single mode ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_41Cycles5); //Enable ADC1 ADC_Cmd(ADC1, ENABLE); //Enable ADC1 reset calibration register ADC_ResetCalibration(ADC1); //Check the end of ADC1 reset calibration register while(ADC_GetResetCalibrationStatus(ADC1)); //Start ADC1 calibration ADC_StartCalibration(ADC1); //Check the end of ADC1 calibration while(ADC_GetCalibrationStatus(ADC1)); //Start ADC1 Software Conversion ADC_SoftwareStartConvCmd(ADC1, ENABLE); //wait for conversion complete while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC)){} //read ADC value AD_value=ADC_GetConversionValue(ADC1); //clear EOC flag ADC_ClearFlag(ADC1, ADC_FLAG_EOC); printf(''\r\n ADC value: %d \r\n'', AD_value); TemperatureC = (uint16_t)((V25-AD_value)/Avg_Slope+25); printf(''Temperature: %d%cC\r\n'', TemperatureC, 176); //read internal temperature sensor end2014-01-28 6:49 AM
There is no forever loop here.
Is it reading one time correctly ? Cheers, Hal2014-01-28 3:54 PM
Yes it's reading it correctly,
I put while(1){} at the end, but it's reading only one time, the next one is empty, do you have idea what the cause is ? thanks2014-01-28 6:07 PM
A more considered presentation might look like this :
void TempSensorInit(void)
{
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
//ADC1 configuration
//select independent conversion mode (single)
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
//We will convert single channel only
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
//we will convert one time
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
//select no external triggering
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
//right 12-bit data alignment in ADC data register
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
//single channel conversion
ADC_InitStructure.ADC_NbrOfChannel = 1;
//load structure values to control and status registers
ADC_Init(ADC1, &ADC_InitStructure);
//wake up temperature sensor
ADC_TempSensorVrefintCmd(ENABLE);
//ADC1 channel16 configuration
//we select 5 cycles conversion for channel16
//and rank=1 which doesn't matter in single mode
ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_41Cycles5);
//Enable ADC1
ADC_Cmd(ADC1, ENABLE);
//Enable ADC1 reset calibration register
ADC_ResetCalibration(ADC1);
//Check the end of ADC1 reset calibration register
while(ADC_GetResetCalibrationStatus(ADC1));
//Start ADC1 calibration
ADC_StartCalibration(ADC1);
//Check the end of ADC1 calibration
while(ADC_GetCalibrationStatus(ADC1));
}
void TempSensorRead(void)
{
//Start ADC1 Software Conversion
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
//wait for conversion complete
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC)){}
//read ADC value
AD_value=ADC_GetConversionValue(ADC1);
//clear EOC flag
ADC_ClearFlag(ADC1, ADC_FLAG_EOC);
printf(''
ADC value: %d
'', AD_value);
TemperatureC = (uint16_t)((V25-AD_value)/Avg_Slope+25);
printf(''Temperature: %d%cC
'', TemperatureC, 176);
}
main(void)
{
//..
TempSensorInit();
while(1)
{
TempSensorRead();
}
}
You'll need to add back your variables, etc.
Try to post sufficiently complete code that demonstrates your problem, not random chunks with a poorly described context and use case.
2014-01-28 11:24 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.