2023-05-18 2:09 AM
Hello,
I succefully figured out to scan ADC1 and ADC2 (countinous mode) with DMA. The issue is that by doing above, controller remains busy and no counter update in while(1). If I disable the ADC start then counter starts working. could you please help me to resolve.
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1); //start the timer
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1); //COMPLEMENTRY OPUTPUT
HAL_TIM_OC_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim8, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim8, TIM_CHANNEL_1); //COMPLEMENTRY OPUTPUT
HAL_TIM_OC_Start(&htim8, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim20, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim20, TIM_CHANNEL_1); //COMPLEMENTRY OPUTPUT
HAL_TIM_Base_Start_IT(&htim3); // this will start the interrupt for core algo
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
HAL_ADC_Start (&hadc2); //START ADC2 BEFORE ADC2 IN MULTIMODE .. ADC2 Ch 1,2
HAL_ADCEx_MultiModeStart_DMA (&hadc1, (uint32_t*)ADC1Samples, //DUAL OPERATION OF ADC1 AND ADC2 .... ADC1 Ch 3,4
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
counter +=1;
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.