2013-04-14 8:31 AM
Dear all:
I have been using the STM32F4 Discovery for few weeks by exploring examples related to DMA and ADC (e.g.,ADC_Interleaved_DMAmode2,TripleADC_Interleaved_DMAmode2, etc). I tried to use these codes in FreeRTOS. The output is attached. It seems that the conversion is only done once and the values were never moved to the buffer through DMA. In FreeRTOS, the ADCtask is shown below. If I dont use DMA with ADC, then it works. Could anyone give some suggests?//Task to handle ADC conversion
static void AdcTask(void *pvParameters){
/* Block for 500ms. */
const portTickType xDelay = 500 / portTICK_RATE_MS;
int i=0;
/* Private define ------------------------------------------------------------*/
#define ADC_CDR_ADDRESS ((uint32_t)0x40012308)
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable peripheral clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_ADC2 |
RCC_APB2Periph_ADC3, ENABLE);
/* Configure ADC Channel 12 pin as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* DMA2 Stream0 channel0 configuration */
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC_CDR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCTripleConvertedValue;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 3;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/******************************************************************************/
/* ADCs configuration: triple interleaved with 5cycles delay to reach 6Msps */
/******************************************************************************/
/* ADC Common configuration *************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_TripleMode_Interl;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_2;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC1 regular channel 10 configuration ************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
/* ADC1 Init ****************************************************************/
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel 10 configuration ************************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 1, ADC_SampleTime_480Cycles);
/* ADC2 Init ****************************************************************/
ADC_Init(ADC2, &ADC_InitStructure);
/* ADC2 regular channel 10 configuration */
ADC_RegularChannelConfig(ADC2, ADC_Channel_10, 1, ADC_SampleTime_480Cycles);
/* ADC3 Init ****************************************************************/
ADC_Init(ADC3, &ADC_InitStructure);
/* ADC3 regular channel10 configuration *************************************/
ADC_RegularChannelConfig(ADC3, ADC_Channel_10, 1, ADC_SampleTime_480Cycles);
/* Enable DMA request after last transfer (multi-ADC mode) ******************/
ADC_MultiModeDMARequestAfterLastTransferCmd(ENABLE);
/* Enable ADC1 **************************************************************/
ADC_Cmd(ADC1, ENABLE);
/* Enable ADC2 **************************************************************/
ADC_Cmd(ADC2, ENABLE);
/* Enable ADC3 **************************************************************/
ADC_Cmd(ADC3, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
while(1){
printf(''%d : %d %d %d\t'', i++, ADCTripleConvertedValue[0]&0xfff,
ADCTripleConvertedValue[1]&0xfff,
ADCTripleConvertedValue[2]&0xfff);
printf(''%d %d %d\n\r'', ADC_GetConversionValue(ADC1)&0xfff, ADC_GetConversionValue(ADC2)&0xfff, ADC_GetConversionValue(ADC3)&0xfff);
// Wait for the next cycle.
vTaskDelay( xDelay );
}
}
#adc-dma-freertos
2013-04-15 3:19 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.