2014-06-16 8:35 AM
2014-06-16 8:57 AM
Not sure I have time to go over this completely, but the most obvious issues are:
tinit.TIM_Period = (84000000 / 553) - 1; // 152 KHz Should betinit.TIM_Period = (84000000 / 152000) - 1; // 152 KHz
(number of ticks at 84MHz for a 152KHz period) Stream ONE so IF1, not IF0void DMA2_Stream1_IRQHandler(void)
{
if(DMA_GetITStatus(DMA2_Stream1, DMA_IT_HTIF1)) {
DMA_ClearITPendingBit(DMA2_Stream1, DMA_IT_HTIF1);
STM_EVAL_LEDOff(LED2);
}
if(DMA_GetITStatus(DMA2_Stream1, DMA_IT_TCIF1)) {
DMA_ClearITPendingBit(DMA2_Stream1, DMA_IT_TCIF1);
STM_EVAL_LEDOn(LED2);
}
}
Describes only half the buffer, the point is to describe the whole buffer and have interrupts at each half (HT/TC)dinit.DMA_BufferSize = SAMPLES_BUFFER_HALF;
Should bedinit.DMA_BufferSize = SAMPLES_BUFFER;
TIM2 is on APB1 NOT AHB1// Enable peripheral clocks
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOA
| RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOF
| RCC_APB1Periph_TIM2, ENABLE);
2014-06-16 9:22 AM
Hi Clive1,
1. Yeah, I blew the period - not worth explaining.2. Yeah, missed the correct stream number for the ADC3 DMA ISR.3. Buffer size, yeah.4. And of course, the biggie! That TIM2 peripheral clock mistake! One lousy character - though it is more than one bit - and everything is broken!Thanks to you, everything now appears to be working correctly!Best regards,Bob2014-06-16 9:43 AM
Not sure it matters to my app, but the TIM2 interrupt doesn't appear to be happening. Is it possible to generate interrupts using
TIM_IT_Trigger
? Or am I missing yet something else? Excerpts:NVIC_InitTypeDef ninit;
TIM_TimeBaseInitTypeDef tinit;
. . .
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
. . .
ninit.NVIC_IRQChannel = TIM2_IRQn;
ninit.NVIC_IRQChannelPreemptionPriority = 0;
ninit.NVIC_IRQChannelSubPriority = 0;
ninit.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&ninit);
. . .
TIM_TimeBaseStructInit(&tinit);
tinit.TIM_Period = (84000000 / 152000) - 1; // 152 KHz
tinit.TIM_Prescaler = 0;
tinit.TIM_ClockDivision = 0;
tinit.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &tinit);
TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Update); // ADC_ExternalTrigConv_T2_TRGO
TIM_ITConfig(TIM2, TIM_IT_Trigger, ENABLE);
TIM_Cmd(TIM2, ENABLE);
. . .
void TIM2_IRQHandler(void)
{
if (TIM_GetITStatus(TIM2, TIM_IT_Trigger) != RESET) {
TIM_ClearITPendingBit(TIM2, TIM_IT_Trigger);
STM_EVAL_LEDToggle(LED3);
}
}
2014-06-16 9:43 AM
If 152 KHz is critical, you could run the processor at 152 MHz rather than 168 MHz, although this would be problematic for using USB.
2014-06-16 9:49 AM
I don't know, I'd perhaps just use the Update rather than the Trigger, but 152 KHz is getting a bit on the high side to be interrupting unless you have too. I'd probably check the pin was configure right, and then see if can toggle a pin directly with one of the TIM2_CHx pins.
You should also be able to measure the TIM2 frequency indirectly via the HT/TC interrupts. A glance suggests they get called at 1 KHz, so a toggle should give 500 Hz at the LED2014-06-16 10:38 AM
Yeah, you're right - that is too fast! I really just wanted to confirm that TIM2 was running, because at the time I wasn't sure what was broken. So, forget about it.
Thanks for your help!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.