2024-05-04 7:14 AM - edited 2024-05-04 8:48 AM
Hello ,
I am generating PWM wave of 16khz ,by using TIM1 ,the Duty cycle updating from the DMA array in circular mode .
(to generate sinewave ).
And worked as expected . The TIM1 is configured the Trigger (TRGO) to update event.
Now i want to sample ADC with a 124 micro second (as per the PWM frequency)
The TIM1 update event should trigger the ADC ,to sample and need to save the data via DMA.
how to configure it
I triedout some of configuration dosent working correctly
please help me
uint32_t ADC_RES[200];
HAL_ADC_Start_DMA(&hadc, (uint32_t*)&ADC_RES,200);
HAL_ADC_Start_DMA(&hadc, (uint32_t*)&ADC_RES,200);
I have configured as follows , But i didnt get 124 micro second sample why ?
static void MX_ADC_Init(void)
{
/* USER CODE BEGIN ADC_Init 0 */
/* USER CODE END ADC_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC_Init 1 */
/* USER CODE END ADC_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_TRGO;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc.Init.DMAContinuousRequests = ENABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime = ADC_SAMPLETIME_71CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC_Init 2 */
/* USER CODE END ADC_Init 2 */
}
Thanking you
2024-05-08 7:03 AM
Why ?
+
look in src -> xxx_hal_msp.c
2024-05-08 7:31 AM
I am a beginer,I didnt know where it is placed ,i didnt see it on main.c configuration section why i asked ,
I am searching for the solution for the same as said in the post .
Trying adc + Timer alone but not working something wrong with me
2024-05-08 7:51 AM
Ok,
so better first look for some examples from STM :
https://github.com/STMicroelectronics
- there are many, just search and look and learn...
2024-05-08 9:48 AM - edited 2024-05-08 10:09 AM
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.