2010-09-30 8:48 AM
2011-05-17 5:09 AM
Noise and source impedance are significant.
Try using ADC_SampleTime_239Cycles5: Sample time equal to 239.5 cycles which will tolerate higher impedance sources. Otherwise, take multiple readings and average them to remove noise effects.2011-05-17 5:09 AM
2011-05-17 5:09 AM
I am measuring directly a battery which is the most low impedance and most noise free thing on the world
second - I am power supplying the STM32 with LM2575-3.3 and it is the only thing on this line which consumes power I dont see a deviation on measured results , I see a jitter the board I use can be seen on this link2011-05-17 5:09 AM
I can't see a schematic for your board when I follow the link but....
If you are using VCC as reference it will not be very precise especially if you are using a switch mode power supply (LM2575). Your going to have noise with this setup -- so you need to live with it. However some _random_ noise can be good when you over sample and filter and can effectivly get you more resolution e.g. 16 bits. Have a google for ''over sampling'' and maybe ''software ADC filter'' etc.2011-05-17 5:09 AM
I checked the schematic of the board of futurlec which I use
first - there is no Vref pins on 64 pin package microcontroller TM32f103ret6 second - the futurlec board has ferrite bead and 10 uF and 100 nF capacitors in front of VDDA I wonder if I have to power on the internal reference with some bit in the ADC registers - maybe thats why so much jitter ?2011-05-17 5:09 AM
HI All,
Could you please tell how to calibrate the ADC. I am giving input of 3.3v and when i write a code to read PC4 pin, i am getting 4095 so i want to convert this value 3.3v. Please tell me is there any specific formula to calibrate ADC?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.