2011-12-19 1:40 AM
Hi,
ADC resolution is working for ''ADC_Resolution_6b'' and ''ADC_Resolution_12b'' but not working for ''ADC_Resolution_8b'' and ''ADC_Resolution_10b'' resolutions, they're same with 12-bit resolution. Does anyone have an idea? Here's the initilize code;definitions;#define ADC_Resolution_12b ((uint32_t)0x00000000)#define ADC_Resolution_10b ((uint32_t)0x01000000)#define ADC_Resolution_8b ((uint32_t)0x02000000)#define ADC_Resolution_6b ((uint32_t)0x03000000)Code;/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div8; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_20Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_8b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); /* ADC1 regular channel7 configuration *************************************/ ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_480Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE); /* Enable ADC1 DMA */ ADC_DMACmd(ADC1, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); ADC_SoftwareStartConv(ADC1);2011-12-19 5:27 AM
Hi,
Could you add in/* ADC1 Init*/
: ''ADC_InitStructure.ADC_ExternalTrigConv=0x00
'' and see if it is solved? Cheers, STOne-322011-12-19 7:27 AM
Unfortunately, Section 10.4 of the reference manual doesn't show 10 and 8 bit data alignment in regular mode. STOne-32 - strong hint.
It might be that the most significant bit position for 10 and 8 bit is the same as 12 bit. Check if the unused 2 or 4 bits are set to zero for 10 and 8 bit conversions. Cheers, Hal2011-12-20 12:29 AM
Thank you very much STOne-32 and Hal,
Problem is solved by adding''ADC_InitStructure.ADC_ExternalTrigConv=0x00;''
It's working for four different resolutions.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.