2013-04-29 12:24 AM
Hello,
I need circuit, which will be protect ADC input against overvoltage. Also, it should amplification low-level voltage (from sensor for example). Do you have something like this?Thank you.2013-04-29 2:09 AM
For smaller voltages, a series resistor and a zener diode of 3.3 ... 3.6V (or better two in antiparallel configuration), would serve well.
For environments with high EMI load and surges of hundreds of volts (say, inductive loads with large back - EMF), you might need special parts like VDRs or suppressor diodes. After all, you might need to have some expectation about the level, duration and frequency of your events the ADC needs to be protected from.2013-04-30 8:43 AM
Can I use operational amplifier with adjustable gain (for low-level signals) followed by voltage follower (for limiting high-level signals)? If I will be sure that input signal isn´t low-level, I connect this signal directly to voltage follower.
2013-04-30 9:46 AM
The voltage follower isn't necessary if the op amp reference voltage is the same as the processor.
Cheers, HalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.