2008-04-17 2:20 AM
ADC keeps converting on high External trigger??
2011-05-17 3:30 AM
Hi
If you use an external trigger for ADC-trigger, the ref-manual says that the ADC will start the conversion on a rising edge, and it is true. If the external trigger signal then stay high, will the ADC then keep converting untill the triggersignal is set to low, even though the ADC is not set to continus mode? -Boelskov2011-05-17 3:30 AM
ADC will start the conversion on a rising edge:
Can't tell if you are questioning the ref manual - it appears that you HAVE generated a rising edge - but of uncertain/unspecified duration. Seems easy to prolong this signal and simply observe... Months ago we capacitor coupled to this trigger pin - eliminating a too-wide input. (our notes don't show IF multiple readings resulted - although one fellow thinks he recalls we had ''accuracy/stability'' issue) You will get the best answer with a small, simple Eval Bd - should you not have your Bd. done. We try to have a small group read a chapter - generate questions - and then we confirm and document on multiple parts multiple boards. Finally - we used a Cpld to emit ''high-going'' one-shot into the STM trigger. Readings are dead stable.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.