cancel
Showing results for 
Search instead for 
Did you mean: 

ADC_GetConversionValue(ADC) == 0 ??

samed
Associate II
Posted on February 06, 2014 at 21:35

Hi I'm getting sometimes 0 from my ADC conversation but this can't be possible.

Pls correct me pls if I say something wrong. I'm working with the STM3210E-Eval board it has an STM32F103GT processor. This is my configuration for my adc1 , I have 3 ADC's because it is the same I'm just posting one.


void
Config_ADC(GPIO_InitTypeDef *GPIO_InitStructure)

{

RCC_ADCCLKConfig(RCC_PCLK2_Div6); 
//clock for ADC ADCCLK = PCLK2/6 = 72/6 = 12MHz*/


// enable ADC system clock

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO | RCC_APB2Periph_ADC1 | RCC_APB2Periph_ADC2 | RCC_APB2Periph_ADC3, ENABLE);


/* Configure PC.01, PC.02 and PC.03 (ADC Channel 11, ADC Channel 12, ADC Channel 13) as analog input */

GPIO_InitStructure->GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ; 
// PC.01, PC.02 and PC.03

GPIO_InitStructure->GPIO_Mode = GPIO_Mode_AIN; 
// Input-Mode

GPIO_InitStructure->GPIO_Speed = GPIO_Speed_50MHz; 
// Speed of port

GPIO_Init(GPIOC, GPIO_InitStructure); 
// apply configuration on PortC


}

ADC_InitStructure->ADC_ContinuousConvMode = ENABLE; 
//ster next convert automatically

ADC_InitStructure->ADC_DataAlign = ADC_DataAlign_Right; 
//put left/right adjusted in register

ADC_InitStructure->ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; 
//choose which extern signal should start convert

ADC_InitStructure->ADC_Mode = ADC_Mode_Independent;

ADC_InitStructure->ADC_NbrOfChannel = 1;

ADC_InitStructure->ADC_ScanConvMode = DISABLE;


ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 1, ADC_SampleTime_28Cycles5);

ADC_Init(ADC1, ADC_InitStructure); 
//set config of ADC1


ADC_Cmd(ADC1, ENABLE); 
1.
//start-callibration 
2.
ADC_ResetCalibration(ADC1); 
/* Enable ADC1 reset calibration register */
3.
while
(ADC_GetResetCalibrationStatus(ADC1)); 
/* Check the end of ADC1 reset calibration register (Reset previous calibration)*/
4.
ADC_StartCalibration(ADC1); 
/* Start ADC1 calibration */
5.
while
(ADC_GetCalibrationStatus(ADC1)); 
/* Check the end of ADC1 calibration */
6.
//End-callibration
7.
8.
ADC_SoftwareStartConvCmd(ADC1, ENABLE);

 

So that means one AD conversion takes 3,41 us. I have an Timer that is active every 30us active.


void
Config_Timer_TIM2(TIM_TimeBaseInitTypeDef *TIM_TimeBaseStructure, NVIC_InitTypeDef *NVIC_InitStructure)

{

// enable TIMER TIM2 system clock

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);



/* Enable the Timer2 Interrupt */

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);


NVIC_InitStructure->NVIC_IRQChannel = TIM2_IRQn; 
// configure the Timer2 interrupts

NVIC_InitStructure->NVIC_IRQChannelPreemptionPriority = 3; 
// sets the priority group of the TIMER2 interrupts

NVIC_InitStructure->NVIC_IRQChannelSubPriority = 0; 
// set the subpriority inside the group

NVIC_InitStructure->NVIC_IRQChannelCmd = ENABLE; 
// TIMER2 interrupts are globally enabled

NVIC_Init(NVIC_InitStructure); 


/* Configure Timer which is every 1 ms active*/

TIM_DeInit(TIM2);

TIM_TimeBaseStructInit(TIM_TimeBaseStructure);


/* Time base configuration */

TIM_TimeBaseStructure->TIM_Prescaler = 72 - 1; 
// 72 MHz / 72 = 1 Mhz


TIM_TimeBaseStructure->TIM_Period = 30 - 1; 
// (1/1Mhz) * 30 = 30 us;

TIM_TimeBaseStructure->TIM_ClockDivision = TIM_CKD_DIV1;

TIM_TimeBaseStructure->TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM2, TIM_TimeBaseStructure);



/* Enable TIM2 Update Interrupt */

TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);


/* Enable TIM2 */

TIM_Cmd(TIM2,ENABLE); 

}

In my Interrupt:


void
TIM2_IRQHandler(
void
)

{

if
(TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)

{ 

if
(calibration < calibration_counter)

{ 

array1 =ADC_GetConversionValue(ADC1); 

array2 =ADC_GetConversionValue(ADC2); 

array3 =ADC_GetConversionValue(ADC3); 

TIM_ClearITPendingBit(TIM2, TIM_IT_Update); 
//Update Interrupt

}

}

}

When I'm getting 512 times an value with ADC_GetConversionValue(ADC) , about 200 values from ADC 3 are 0 , from ADC2 are 139 zero and ADC1 are 56 zero. What is the problem ? #adc
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on February 06, 2014 at 21:49

Yeah, well that's practically unreadable. Just cut-n-paste the source into the Format Code Block window, it doesn't recognize HTML

You don't seem to qualify the EOC status prior to reading the values. In understanding the cases where you read zero, you might want to check the status of the ADC. If you ground the pin you might expect to see a zero.

Might make more sense to trigger the ADC with the timer.

Clear the update interrupt prior to reading the ADC values.

Post COMPLETE code.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on February 07, 2014 at 00:37

So the EOC is not a fixed period of time ? I thought a

ADC_SampleTime_28Cycles5

with 12 Mhz is one ADC about 3,41 us long...

Even if I do to wait for EOC the result is the same...

while

(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

// Get the conversion value

array1= ADC_GetConversionValue(ADC1);   while

(ADC_GetFlagStatus(ADC2, ADC_FLAG_EOC) == RESET); array2= ADC_GetConversionValue(ADC2);

while

(ADC_GetFlagStatus(ADC3, ADC_FLAG_EOC) == RESET); array3= ADC_GetConversionValue(ADC3); 

raptorhal2
Lead
Posted on February 07, 2014 at 20:01

The problem might be outside the posted information.

Is there more than ADC conversion happening in the code ?

What are the three signal sources, and how are the grounds connected between the Eval board and the signal sources ?

Are the signal sources monitored with a scope or meter ?

Are any jumpers between BNC1-3 and PC1-3 different from the Eval board delivered configuration ?

Cheers, Hal

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.