2014-10-04 10:08 AM
They are aliases of channels 15,17,17,17 for ADC 1-4 correspondingly. According to STM32F303VC reference they should by aliases of channels 3,3,1,3. Firmware works correctly only when they are set according to reference.
stm32f3xx_hal_adc_ex.h is version V1.0.1 from 18-June-2014 #stm32f303vct6-stm32cubef32014-10-06 9:48 AM
Hello Alexander,
ADC_CHANNEL_VOPAMPx are the reference voltage for the OPAMPx connected to ADC. If you refer to RM0316:- ADC1_IN15 = VREFOPAMP1= Reference Voltage for the Operational Amplifier 1- ADC2_IN17 = VREFOPAMP2= Reference Voltage for the Operational Amplifier 2- ADC3_IN17 = VREFOPAMP3= Reference Voltage for the Operational Amplifier 3- ADC4_IN17 = VREFOPAMP4= Reference Voltage for the Operational Amplifier 4If you need to use OPAMP output as ADC inputs, the other channels (ADC1_IN3, ADC2_IN3, ADC3_IN1, ADC4_IN3) have to enabled.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-10-07 8:40 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.