2013-11-05 3:59 AM
Hello,
I
'm using stm32f
417vg chip and arm-none-eabi-gcc compiler
(and gd
b
).
I try to get adc
to read 14an
alog
input
channels
.
Channels 1, 2
, 3
values are fine, b
ut
wh
en i
re
ad ch
annel
4
value
doe
sn't change at all.
I use code below:
typedef struct { GPIO_TypeDef* port; uint32_t pin; }gpioConfigs_t; static gpioConfigs_t gpioConfig[] = { {GPIOA,GPIO_Pin_1}, {GPIOA,GPIO_Pin_2}, {GPIOA,GPIO_Pin_3}, {GPIOA,GPIO_Pin_4}, {GPIOA,GPIO_Pin_5}, {GPIOA,GPIO_Pin_6}, {GPIOA,GPIO_Pin_7}, {GPIOB,GPIO_Pin_0}, {GPIOB,GPIO_Pin_1}, {GPIOC,GPIO_Pin_0}, {GPIOC,GPIO_Pin_1}, {GPIOC,GPIO_Pin_2}, {GPIOC,GPIO_Pin_3}, {GPIOC,GPIO_Pin_4} }; void internalAdc_init2(void) { GPIO_InitTypeDef GPIO_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; ADC_InitTypeDef ADC_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE); for(i = 0; i < INTERNAL_ADC_CHANNELS; i++){ GPIO_InitStructure.GPIO_Pin = gpioConfig[i].pin; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(gpioConfig[i].port, &GPIO_InitStructure); } ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC3 Init */ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC3, &ADC_InitStructure); /* Enable ADC3 */ ADC_Cmd(ADC3, ENABLE); } uint16_t readAdc(uint8_t channel) { uint16_t res, val = 0; ADC_RegularChannelConfig(ADC3, channel, 1, ADC_SampleTime_3Cycles); ADC_SoftwareStartConv(ADC3); while(ADC_GetFlagStatus(ADC3, ADC_FLAG_EOC) == RESET); val = ADC_GetConversionValue(ADC3); res = val >> 4; return res; }from app ->
uint16_t test
Data;
testData = readAdc(1); /*ok
*/ testData = readAdc(2); /* ok */ testData = readAdc(3);/*ok *
/
testData = readAdc(4);/* This valued
oes
not chan
ge
*/2013-11-05 5:05 AM
PA4 ADC12_IN4 has NO associativity with ADC3 (just 1 and 2), refer to the
http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1577/LN11/PF252139
.2013-11-05 6:41 AM
Ahh i was missread specs for that part. Thank you very much for help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.